Optical Image Stabilization (OIS) Explained: Types and Working

Optical Image Stabilization as Fast As Possible
Catalog
ⅠTypes of Image Stabilization
The effect of optical image stabilization is quite obvious. Normally, this function can improve the 2-3 gear shutter speed, so that the handset does not produce an ambiguous phenomenon, which is very obvious for beginners. In addition, in the telephoto type digital camera, optical image stabilization also works.
OIS is an anti-shake technology that is most recognized by the public, which is compensated by a movable part, thereby achieving an effect of alleviating photos blur. The optical image stabilization technique is divided into two major factions, namely the lens mobile optical image stabilization of the lens manufacturer, and CCD mobile optical image stabilization represented by emerging electronic vendors. However, since optical image stabilization needs to be implemented using additional components, it also leads to the high cost of optical image stabilization systems, and the model market selling the optical image stabilization system is still more expensive.
1.Lens-based image stabilization

Camera module with optical image stabilization (OIS)
Through the lens group, the image stabilization is mainly based on Canon and Nikon, which rely on magnetically packaged suspensions, thereby effectively overcoming image blur due to camera vibration, which is more obvious to the digital camera of the large zoom lens. Typically, the gyroscope inside the lens detects tiny movement and transmits the signal to the microprocessor immediately. The microprocessor calculates the displacement amount that needs to be compensated. Then the light path will pass through the compensation lens group. According to the shake direction and displacement of the lens, the compensation lens group will adjust the position and angle accordingly to keep the optical path stable, thereby efficiently overcoming the imaging blur of the camera shack.
2.CCD image stabilization
The image stabilization is achieved by CCD, which is the purpose of relying on the CCD to achieve anti-shake. The principle is to secure the CCD first on a bracket that can move up and down. Sensing the direction and amplitude of camera shake through the gyroscope, and then transmits these data to the processor for screening, enlarges. The processor finally calculates the amount of CCD movable to cancel the shack.
3.Electronic image stabilization
The so-called electronic image stabilization (EIS), that is, the whole process of image stabilization does not have any component assistance and participation, relying on digital processing technology to achieve image stabilization. The current electronic image stabilization mainly is achieved by two types of technologies. One is to increase camera sensitivity (ISO) and another is "digital image stabilization" achieved by pixel compensation or other operational methods.
4.Dual image stabilization
The so-called "double image stabilization" is a digital camera image stabilization system consisting of two technologies of "optical image stabilization" and "high sensitivity". Among them, optical image stabilization is a more complex technique, which relies on the camera's built-in precision gyroscope and a set of movable lenses to calculate and correct the light offset caused by the hand. The principle of “high sensitivity” is relatively simple, which is to improve the shutter speed by increasing the sensitivity ISO value, and can also achieve the image stabilization effect.
Ⅱ Working principle of Optical Image Stabilization
1.Lens-based optical image stabilization
The first optical image stabilization system for civilian cameras in the world is developed by Canon. EF 75-300mm F4-5.6 IS USM lens is the first application of an optical image stabilization system on a civilian camera. At the time, the industry was indeed shocked throughout the industry, and the visibility of the Canon EF autofocus lens gradually increased, which is called Canon's IS (Imagine Stabilizer) optical image stabilization system. It is mainly to compensate for the shake of the camera through the movement of the lens. In Canon's image stabilization lens, it is equipped with a gyro sensor. It can accurately detect the vibration of the hand and convert it into an electrical signal. After the built-in computer processing, control a set of modified optical components as a film or CCD. The plane is moving in parallel, offset the imaging light shift due to the hand shock. This system can effectively improve the effect of handheld shooting.

Optical image stabilization internal structure
The Canon IS lens can detect the shake of the camera through a pair of built-in gyroscope sensors, and adjust the lens assembly to the direction of jitter to cancel this jitter to prevent the picture from blurring. If the image stabilization function is enabled, the camera will start the camera jitter compensation after 0.5 seconds. The lens with IS can theoretically reduce the second to three-level shutter speeds. Since the potential optical performance of the lens is optimized, you can capture a beautiful image.

Optical image stabilization principle
In the past, IS lenses allowed you to use a shutter speed that was 2 levels lower than the theoretical shutter speed. As this technique is constantly developing, it is already possible to use shutter speeds 3 levels lower than the theoretical shutter. On the latest release of Canon EF 70-200mm f / 4l USM, Canon's latest generation IS optical image stabilization system is equipped, theoretically reduces the 4-speed shutter speed, which is the king of the image stabilization lens.
2.Sensor-shift optical image stabilization
Since the lens-based optical anti-shake is high in production technology and cost, some manufacturers developed the sensor-shift optical anti-shake (CCD anti-shake) system. This technique has occurred as the digital camera appears because its principle determines that the film machine cannot be imitated in this way.
The principle of sensor-shift optical image stabilization is much simpler than Lens-based optical image stabilization. That is to fix the photosensitive element (CCD / CMOS) of the digital camera on a platform that can slide through the electromagnetic effect. When shooting, the platform will use the hysteresis of the electromagnetic to fix the CCD in a short period of time, which is reached to some extent the purpose of anti-shake.
CCD optical image stabilization technology is first known as the AS (Anti Shake) system developed by Konica, and is first applied to its high-end consumption digital camera A1, and has received excellent market effects. Since then, Konica Beauty can transplant this technology to digital SLR α7 Digital and α5 Digital, and receive a warm welcome from the market. This technology is also mastered by Sony Machine in Konica Merco-up imaging. Due to the late development of this technology, the technology is not as mature as the lens anti-shake. But with the continuous introduction of new models of various brands, its image stabilization performance has also been steadily improved, and it has great momentum to catch up with the lens-based image stabilization. For example, Pentax’s newly released SLR digital camera K10D claims to be able to achieve level 3 anti-shake, which is a level higher than the level 2 anti-shake of its predecessor K100D.
1.What does optical image stabilization do?
Optical image stabilization prolongs the shutter speed possible for handheld photography by reducing the likelihood of blurring the image from shake during the same exposure time.
2.Which is better EIS or OIS?
OIS primarily improves low light photography by physically compensating for handshake within every single frame, and EIS improves shaky video by maintaining a consistent framing between multiple video frames. OIS is primarily for photos, and EIS is only for video.
3.What is the OIS feature?
(OIS) A technology for cameras that physically moves the camera lens or sensor to compensate for unintentional camera movement. Any time a camera takes a photo, the image is captured over a period of time. That period of time is extremely short when working with ample light.
4.What is OIS on phone?
Samsung's Optical Image Stabilization system, or OIS, uses a combination of hardware and software processing that's advanced enough to deliver clear and sharp photos even in low light thanks to the big sensor on the Galaxy S and Note series.
5.Does OIS make a difference?
OIS is a useful tool to have whether you are shooting video or photos. It's particularly adept in low-light scenarios, where the camera's shutter may be open for longer. Without OIS, this can result in blurry photos due to slight hand movement.
6.What is the difference between optical and digital image stabilization?
Unlike optical systems, digital image stabilization — also called electronic image stabilization — uses software to reduce blur. Some camcorders calculate the effect of your body movement and use that data to adjust which pixels on the camcorder's image sensor activate.
7.What is the work of OIS?
OIS is a mechanical technique used in imaging devices to stabilize the recording image by controlling the optical path to the image sensor. The two main methods of OIS in compact camera modules are implemented by either moving the position of the lens (lens shift) or the module itself (module tilt).
8.How important is optical image stabilization?
For night photographers or low light photography, image stabilization helps considerably. It allows photographers to use a shutter speed that is 2 to 4.5 stops slower to capture sharp and detailed images despite having less light.
9.Do I need optical image stabilization?
So really, image stabilization is the most important in situations where you don't have enough light to get a fast shutter speed. It tends to come in handy at sunset, sunrise, and indoors. In most cases, image stabilization will give you the same image quality at 3 to 4 shutter speed stops slower than usual.
10.When should I turn off image stabilization?
While the slow-speed limits may vary slightly from one lens model to another, Image Stabilization is disabled if the system detects a shutter speed longer than roughly one full second. So for longer night-time exposures, expect to just turn IS off, because it won't have an effect on your final pictures.
The Introduction to Common Tools and Using Methods of Fiber OpticUTMEL07 January 20226678The building and maintenance of optical cables in the intelligent industry has gradually expanded with the rapid expansion of the Internet of Things and 5G technologies, resulting in an increase in demand for various optical fiber tools. Cutting shears, for example, come in a variety of shapes and sizes, and each tool serves a different purpose. Do you have any experience with them? When should you utilize certain fiber optic tools?
Read More
What are Fiber Optic Patch Cables?UTMEL11 February 20227805Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.
Read More
Basis of Fiber Optic and Fiber Optic CommunicationUTMEL22 October 20214732Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.
Read More
The History of MicroscopeUTMEL21 October 20217543Hello, everyone. I am Rose. Today I will show you the history of microscopes. The microscope is used to magnify tiny objects into instruments that can be seen by human eyes. Microscopes are divided into optical microscopes and electron microscopes.
Read More
What is VCSEL?UTMEL28 October 202111334Hello everyone, I am Rose. I welcome you on board, today I will introduce VCSEL to you. The Vertical-Cavity Surface-Emitting Laser (VCSEL, or Vertical-Cavity Surface-Emitting Laser) is a semiconductor whose laser is emitted perpendicular to the top surface. It differs from an edge-fired laser, which emits the laser from the edge.
Read More
Subscribe to Utmel !
SML-H12M8TT86ROHM Semiconductor
HFBR-2416TZBroadcom Limited
HLMP-1700Broadcom Limited
SMLP34RGB1W3ROHM Semiconductor
QED234ON Semiconductor
IR908-7C-FEverlight Electronics Co Ltd
LNJ447W84RA1Panasonic Electronic Components
HFBR-2412ZBroadcom Limited
12-215UYC/S530-A3/TR8Everlight Electronics Co Ltd
HFBR-2505AFZBroadcom Limited


Product
Brand
Articles
Tools