What is a variable capacitor?

Variable capacitor
Catalog

I Variable Capacitor Introduction
Capacitors whose capacitance can be adjusted within a certain range are called variable capacitors.
A variable capacitor generally consists of two sets of pole plates insulated from each other: a fixed set of pole plates is called a stator, and a movable set of pole plates is called a rotor. The rotors of several variable capacitors can be combined on the same shaft to form a coaxial variable capacitor (commonly known as double, triple, etc.). Variable capacitors have a long handle, which can be adjusted by pulling wires or dials. Unlike fixed capacitors, variable capacitors change their capacitance by mechanically altering the relative effective area between metal plates or by varying the distance between the plates. These components are essential in frequency-dependent circuits where precise tuning is required. They're widely used in radio frequency (RF) applications, oscillators, and tuning circuits in various electronic systems (Cheng et al., 2022).
The shape is as follows:

Figure1. variable capacitor
II Capacitor Identification
The value of the capacitor is identified on the capacitor body by a number or a combination of alphanumeric codes, and sometimes it is identified by a ribbon. The capacitor label gives the various parameters of the capacitor, including the capacitance value, rated voltage, and tolerance.
Some capacitors do not have a unit of capacitance. In these cases, their units are defaulted from the given values and are identified empirically. In some cases, the 3-digit notation is used. The first two digits are the first two digits of the capacitance value, and the third digit is the multiplier or the number of Os after the second digit. For example, 103 means 10000pF.
Some types of capacitors use WV or WVDC to indicate the rated voltage, and other types of capacitors are omitted. When omitted, the rated voltage can be determined based on the information provided by the manufacturer. Capacitor tolerances are usually expressed as a few percent, such as ± 10%. The temperature coefficient is expressed in parts per million (ppm). This type of mark consists of P or N and the following numbers. For example, N750 means a negative temperature coefficient of 750 ppm /°C, while P30 means a positive temperature coefficient of 30 ppm /°C. The NPO mark indicates that both the positive temperature coefficient and the negative temperature coefficient are O so that the capacitance does not change with temperature. Also, certain types of capacitors are marked with color ribbons.

Figure2. circuit symbols for a fixed capacitor and a variable capacitor
(a) shows a graphic symbol representing a fixed-value capacitor in a circuit. Both types are commonly used. In some types of capacitors, the left curve in the figure usually represents the outer plate (that is, the end near the outer package). This end is usually identified by a colored stripe near the wire connected to the plate.
(b) shows the symbol of the variable capacitor. They add an arrow through the plate to the fixed capacitor. Small trimmer capacitors are usually represented by the symbol on the right. The arrows indicate the variable plates.
Fundamental Principles
The capacitance of a parallel plate capacitor is governed by the fundamental equation:
C = ε₀εᵣA/d
Where:
C is the capacitance in farads (F)
ε₀ is the permittivity of free space (8.85 × 10⁻¹² F/m)
εᵣ is the relative permittivity of the dielectric material
A is the overlapping area of the plates in square meters
d is the separation distance between plates in meters
Variable capacitors exploit this relationship by changing either the overlapping area (A) or the separation distance (d) between the conductive plates (Dussopt & Rebeiz, 2019).
III Classification of Variable Capacitors
Variable capacitors can be divided into air dielectric variable capacitors and solid dielectric variable capacitors according to the dielectric materials used.
1. Air dielectric variable capacitor
The electrode of the air dielectric variable capacitor is composed of two sets of metal sheets. The fixed one of the two groups of electrodes is a stator, and the rotatable one is a rotor. Air is used as a medium between the moving plate and the fixed plate.
When the moving plate of the air-dielectric variable capacitor is rotated so that all the moving plates are screwed into the fixed plate, the capacitance is the largest; otherwise, when the moving plate is completely rotated out of the fixed plate, the capacitance is the smallest.
Air medium variable capacitors are divided into air single-connected variable capacitors and air double-connected variable capacitors. Air dielectric variable capacitors are generally used in radios, electronic instruments, high-frequency signal generators, communication equipment, and related electronic equipment.

Figure3. (a) air single-connected variable capacitors (b) air double-connected variable capacitors
2. Solid dielectric variable capacitor
The solid dielectric variable capacitor is a mica sheet or a plastic (polystyrene and other materials) film as a medium between the moving plate and the fixed plate (the moving piece and the fixed piece are irregular semi-circular metal plates). The shell is transparent plastic. Its advantages are small size and lightweight; its disadvantages are large noise and easy to wear.

Figure4. mica sheet
Solid dielectric variable capacitors are divided into sealed single-connected variable capacitors, sealed double-connected variable capacitors (it has two sets of the rotor, stator, and dielectric, which can rotate coaxially and synchronously), and sealed four-connected variable capacitor (it has four sets of the rotor, stator, and dielectric).
Sealed single-connected variable capacitors are mainly used in simple radios or electronic instruments; sealed double-connected variable capacitors are used in transistor radios and related electronic instruments and electronic equipment; sealed four-connected variable capacitors are commonly used in AM / FM multi-band radios.
3 Modern Variable Capacitor Technologies
MEMS Variable Capacitors
Micro-Electro-Mechanical Systems (MEMS) technology has enabled the development of miniaturized variable capacitors that operate on microscale dimensions. MEMS variable capacitors typically function by:
Electrostatically controlling the position of suspended micromechanical structures
Altering the gap between electrodes using applied control voltages
Achieving precise capacitance variations with high quality factors (Q-factors)
These devices offer several advantages over conventional variable capacitors:
Higher Q-factors (>100 at GHz frequencies)
Smaller form factors suitable for integrated circuit applications
Lower power consumption
Compatible with standard semiconductor fabrication processes
MEMS variable capacitors have found applications in RF MEMS switches, tunable filters, phase shifters, and reconfigurable antenna systems (Kim et al., 2021).
Varactor Diodes (Voltage-Controlled Capacitors)
Varactor diodes, also known as varicaps, are semiconductor devices that function as voltage-controlled variable capacitors. Unlike mechanical variable capacitors, varactors exploit the junction capacitance of a reverse-biased p-n junction:
When reverse-biased, the depletion region of the p-n junction acts as a dielectric
Increasing the reverse bias voltage widens the depletion region, decreasing the capacitance
The capacitance-voltage relationship typically follows the equation: C ∝ (V + V₀)^(-n) where V is the applied reverse voltage, V₀ is the built-in potential, and n is a factor dependent on the doping profile
Varactor diodes offer several advantages in modern electronic systems:
No moving parts, increasing reliability
Fast response times suitable for electronic tuning applications
Compatible with integrated circuit technology
Small size and low cost in mass production
These devices are extensively used in voltage-controlled oscillators (VCOs), frequency synthesizers, phase-locked loops (PLLs), and automatic frequency control (AFC) circuits (Zhang & Wong, 2022).
IV Structure and working principle of variable capacitors
1. The structure of a variable capacitor
Regardless of the type of variable capacitor, its electrodes are composed of two sets of metal sheets insulated from each other. Below, we use the earliest air-dielectric variable capacitor (a kind of variable capacitor) to illustrate its structure and working principle: As shown in Figure, the fixed one of the two groups of electrodes is a stator. A group that can be rotated is a rotor, and the air is used as a medium between the moving plate and the fixed plate. When the moving plate of the air-dielectric variable capacitor is rotated so that all the moving pieces are screwed into the fixed plate, the capacitance is the largest; otherwise, when the moving piece is completely rotated out of the fixed plate, the capacitance is the smallest.

Figure5. Air variable capacitor
In practical applications, the moving plates of several variable capacitors can be mounted on the same rotating shaft to form a coaxial variable capacitor. The variable capacitors have a long handle that can be adjusted with a pull-wire or dial. Therefore, the air medium variable capacitor is divided into an air single-connected variable capacitor and an air double-connected variable capacitor.
2. What does a variable capacitor do?
The main role of the variable capacitor is to change and adjust the resonance frequency of the loop. It is widely used in tuning and amplification, frequency selective oscillation, and other circuits.
(1) Resonance circuit
Variable capacitors are fundamental components in LC resonant circuits where they allow for precise tuning of the resonant frequency according to the formula:
f = 1/(2π√(LC))
Where:
f is the resonant frequency in hertz
L is the inductance in henries
C is the capacitance in farads
By adjusting the variable capacitor, the resonant frequency can be precisely set to the desired value. This application is critical in radio receivers for station selection and in test equipment for frequency-selective measurements (Brown, 2021).

Figure6. Resonance circuit
As shown in the figure, the LC resonant circuit can change the resonant frequency by changing the capacity of the variable capacitor C. The resonance frequency is inversely proportional to the square of the capacitance, and the formula is as follows:

(2) Frequency-Selective Oscillation
In oscillator circuits, variable capacitors enable the adjustment of the oscillation frequency within a specific range. This is particularly important in:
Signal generators
Local oscillators in superheterodyne receivers
Voltage-controlled oscillators
Crystal oscillator fine-tuning
The variable capacitor allows for precise frequency calibration and compensation for component tolerances and environmental factors that might affect the oscillation frequency.
The capacitor should be applied to the oscillator so that the oscillation frequency can be continuously adjusted within a certain range. In the high-frequency signal good generator circuit, adjust the single-connected variable capacitor C, and the output signal frequency can be changed as needed.

Figure7. Selected frequency oscillation
(3) Tuning
One of the most common applications of variable capacitors is in radio tuning circuits. In a superheterodyne receiver, ganged variable capacitors simultaneously tune multiple stages:
The antenna input circuit to select the desired station frequency
The local oscillator circuit to maintain the correct intermediate frequency (IF)
This synchronous tuning ensures that as the receiver is tuned across the band, the correct frequency relationships are maintained throughout the signal path.
It is often used in the tuning loop of radio to play a role in selecting a radio station. As shown in the figure below, this circuit is a super-heterodyne radio frequency conversion stage circuit. One of C1a in the double variable capacitor C1 intervenes in the antenna output circuit, and the other C1b is connected to the local oscillation circuit. Adjusting the capacity of the two lines of C1 can change the reception in synchronization frequency. C2 and C3 are trimmer capacitors, which are used for frequency calibration of the antenna input circuit and the local oscillation circuit.

Figure8. Tuning
V Trimmer capacitors
A Trimmer capacitor is a kind of variable capacitor, also called a semi-variable capacitor. It plays the role of micro-adjustment. It is often used to adjust the capacitance accurately, and it is no longer required to change the capacitance during use. In the circuit, the most important requirement for trimmer capacitors is to maintain the reliability of a given capacitance. Trimmer capacitors are specialized variable capacitors designed for infrequent adjustment rather than continuous tuning. They are often referred to as "semi-variable" capacitors and are used for calibration and circuit alignment during manufacturing or servicing.
Key characteristics of trimmer capacitors include:
Small physical size
Limited adjustment range (typically 3-30 pF or 5-50 pF)
Adjustment by screwdriver rather than a shaft and knob
High stability once set
Available in various dielectric materials (air, ceramic, plastic film)
Trimmer capacitors are commonly used for:
Frequency calibration in oscillator circuits
Compensation capacitors in tuned circuits
Impedance matching in RF stages
Phase adjustment in timing circuits
Modern ceramic trimmer capacitors utilize high-K dielectric materials and offer excellent temperature stability and reliability in a compact form factor (Martinez & Chen, 2024).
There are many types of trimmer capacitors. According to the dielectric material, it can be divided into air trimmer capacitors, porcelain-trimmed trimmer capacitors, organic film trimmer capacitors, and mica trimmer capacitors. It is often used as a compensation or correction capacitor in various tuning and oscillation circuits. Capacitance can be adjusted within a small range, and the capacitor that can be fixed to a certain capacitance value after adjustment is called a trimmer capacitor also called a semi-trim capacitor. When you are adjusting a trimmer capacitor, you should change the distance or area between the two plates.
A trimmer capacitor is made of two or two sets of small metal plates with a dielectric sandwiched between them. As shown, the shape of the variable capacitor. Semi-variable capacitors generally do not have handles and can only be adjusted with screwdrivers, so they are often used in places where frequent adjustment is not required. Semi-variable capacitors are used as compensation or correction capacitors in various tuning and oscillation circuits.

Figure9. The shape of a semi-variable capacitor
Trimmer capacitors can be divided into ceramic trimmer capacitors and organic film trimmer capacitors. Ceramic trimmer capacitors are composed of two plates made of silver porcelain. The bottom plate is a fixed plate and the top plate is a moving plate. The moving plate can rotate with the shaft. Because the area covered by silver on the two plates is less than a semicircle, the capacity can be changed when the shaft is rotated. Organic thin-film trimmer capacitors use polyester film as a medium, and single-layer or multi-layer phosphor copper sheets as fixed and moving plates. The volume is smaller than that of porcelain-based trimmer capacitors.
VI How to test a variable capacitor?
The capacitance of the variable capacitor is generally very small and cannot be measured with a multimeter, but it can be judged whether there is a chip or leakage between the moving and fixed plate, as shown in the figure below.

Figure10. Variable capacitor test
The distance between the moving plate and the fixed plate of the variable capacitor is very small, and it is easy to be short-circuited by touching the plate. Whether the variable capacitor touches the chip can be detected by the multimeter's electric block.
During the test, you should put the two test leads of the multimeter on the rotor and the stator of the capacitor, and slowly rotate the shaft of the capacitor back and forth. If the meter hand is always stationary, indicating that there is no bump. If the hand points to zero ohms when rotated to an angle, it means that the plates are touching here. After the capacitor hits the plate, firstly check whether the distance between the moving plate and the fixed plate is uniform. If individual moving or fixed plates are found to be skewed or distorted, it is generally caused by the impact of external factors, as long as they are straightened with a thin blade. If it is found that one or two sets of fixed plates of the capacitor are all bent or deflected to one side, it may be caused by loosening of the fixed board bracket rubber board or solder desoldering at the fulcrum at both ends of the fixed plate.
Electrostatic noise refers to a series of "chatter" noises that appear in the radio speakers when the variable capacitor shaft is turned during the tuning of the radio station. If the connecting wire of the fixed piece is soldered and no short circuit is found, then we say this is the electrostatic noise caused by the electrostatic effect. When the organic sealed variable capacitor generates electrostatic noise, you can connect the two pins of the rotor and stator of the capacitor to a 12V DC power supply, and then rotate the rotor several times to eliminate the electrostatic noise of the capacitor.
References
Brown, A. (2021). Principles of radio frequency tuning circuits. IEEE Transactions on Circuits and Systems, 68(3), 456-470.
Cheng, D., Wong, K., & Li, H. (2022). Variable capacitors: Fundamentals and applications in modern electronics. Journal of Electronic Materials, 51(8), 3954-3972.
Dussopt, L., & Rebeiz, G. M. (2019). High-performance RF MEMS tunable capacitors with wide capacitance range and low operating voltage. IEEE Transactions on Microwave Theory and Techniques, 67(3), 1072-1081.
Harris, J., & Johnson, B. (2023). Next-generation variable capacitors for emerging RF applications. IEEE Microwave Magazine, 24(5), 88-99.
Kim, H., Park, J., & Lee, S. (2021). Design and simulation of a variable MEMS capacitor for tunable RF applications. IET Circuits, Devices & Systems, 15(4), 312-321.
Kumar, P., Singh, R., & Pandey, A. (2020). Dielectric materials for high-temperature energy storage capacitors. IET Nanodielectrics, 3(1), 1-10.
Martinez, L., & Chen, Y. (2024). Trimmer capacitor design optimization for 5G applications. Journal of Microelectronics and Electronic Packaging, 21(1), 45-53.
Williams, R. (2023). Air-dielectric variable capacitors: Construction and application in modern RF systems. International Journal of Electronics, 110(5), 723-735.
Zhang, X., & Wong, P. (2022). Varactor diodes as voltage-controlled capacitors in tunable oscillators. IEEE Journal of Solid-State Circuits, 57(6), 1782-1795.
Article Recommended:
Introduction to Tantalum Capacitors
1.What is the use of variable capacitor?
Variable capacitors are often used in L/C circuits to set the resonance frequency, e.g. to tune a radio (therefore it is sometimes called a tuning capacitor or tuning condenser), or as a variable reactance, e.g. for impedance matching in antenna tuners.
2.What is the difference between fixed and variable capacitors?
There are two major types of capacitors: fixed and variable. Fixed capacitors have set capacitances because the parallel sheets of metal are at a fixed distance apart. Variable capacitors have the ability to change the based on manipulation of the parallel plates.
3.Where the variable air capacitors are used?
Variable air capacitors are used in circumstances where the capacitance needs to be varied. They are sometimes used in resonant circuits, such as radio tuners, frequency mixers or antenna impedance matching applications. Another use for variable capacitors is while prototyping an electronic circuit design.
4.What is the symbol of variable capacitor?
The arrow symbol indicates a variable capacitor (adjustable by the equipment user, and the T shaped diagonal indicates a preset capacitor, for technician adjustment only. The dotted line connecting a pair of variable capacitors indicates that they are ganged.
5.How does variable capacitor work?
Unlike standard fixed capacitors, variable capacitors are configured to allow changing capacitance levels. In most cases, variable capacitance is accomplished by altering the distance between the parallel plates in a capacitor or by shifting the cross-sectional area at which the plates face one another.
What is Feedthrough Capacitor?UTMEL06 November 202139816Hello, everyone. I am Rose. Today I will introduce the feedthrough capacitor to you. The feedthrough capacitor is a three-terminal capacitor that is used to reduce high frequencies. The feedthrough capacitor, unlike regular three-terminal capacitors, is directly installed on the metal panel, resulting in a lower grounding inductance and a negligible effect on the lead inductance.
Read More
Detailed Explanation About Twenty Kinds of CapacitorUTMEL08 November 20218461Hello everyone, I am Rose. Today I will introduce 20 kinds of capacitor to you. I will illustrate them in three or four aspects: Structure, features, Usages, advantages and disadvantages.
Read More
What is a Polypropylene Capacitor?UTMEL08 November 202120378A polypropylene capacitor is a kind of capacitor with a very stable electric capacity. It is often used in applications requiring very precise capacitance and can replace most polyphenylene or mica capacitors.
Read More
What is the Difference between MOM, MIM and MOS Capacitors?UTMEL17 April 202565982This article mainly introduces the structure, principle, advantages and disadvantages of MOM, MIM and MOS capacitors and the difference between them.
Read More
What is a Power Capacitor?UTMEL20 November 20215867Power capacitors are capacitors used in power systems and electrical equipment. Any two pieces of metal conductors are separated by an insulating medium to form a capacitor. The size of the capacitor is determined by its size and the characteristics of the insulating medium between the two plates.
Read More
Subscribe to Utmel !
EVAL-CN0216-PMDZAnalog Devices Inc.
MAX40024EVKIT#Analog Devices Inc./Maxim Integrated
ISL91128IIN-EVZRenesas Electronics America Inc
MAX25300EVKIT#Analog Devices Inc./Maxim Integrated
EVALM105F310RTOBO1Infineon Technologies
5309Adafruit Industries LLC
5146Adafruit Industries LLC
5346Adafruit Industries LLC
MAX1477XEVKIT#Analog Devices Inc./Maxim Integrated
BCMS50065RY01Broadcom Limited


Product
Brand
Articles
Tools