What is a Microcontroller?

Published: 28 May 2020 | Last Updated: 30 October 2025116515
A microcontroller is a sophisticated single-chip microcomputer that integrates all essential computing elements onto a single integrated circuit (IC). Microcontrollers are mainly used for automatic control equipment in the fields of automobile air conditioning and automatic machinery. Microcontrollers are widely used in various industrial and civil embedded systems due to their small size, low power consumption, and ease of use.
This video is intended for beginners unfamiliar with Microcontroller. The basic components of a Microcontroller are compared to a common household PC to help reinforce concepts.

What is a Microcontroller?

Catalog

ⅠWhat is a microcontroller?

Ⅱ Types of microcontroller

Ⅲ What is the difference between a microcontroller and a microprocessor?

 

1 The role of the microcontroller

2 The basic functions of the device controller

3 The difference between a microprocessor and a microcontroller



Micro- controller.png

Ⅰ What is a microcontroller?

At its core, a microcontroller is a compact computing system containing a processor core, memory, and programmable input/output peripherals on a single chip. Unlike general-purpose computers designed to run various applications, microcontrollers are purpose-built for specific control tasks within embedded systems (Valvano, 2019).

Microcontroller

Microcontroller

A microprocessor is a computer. All computers-whether we say a personal desktop computer or a mainframe computer or a microcontroller-have a lot in common:

All computers have a CPU (Central Processing Unit) for executing programs. If you are sitting in front of a desktop computer and reading this article, the CPU of this computer is now executing a program, which is the web browser used to display this web page. The CPU loads the program from a device. On your desktop computer, the browser program is loaded from the hard disk. The computer has some RAM (random access memory) used to store "variables".

Besides, the computer has some input and output devices, so that it can exchange information with the user. On your desktop computer, the keyboard and mouse are input devices, and the monitor and printer are output devices. The hard disk is an input-output device because it can both input and output data.

Key Components of a Microcontroller:

ComponentDescription
Central Processing Unit (CPU)The brain that executes instructions and performs calculations
Memory System
- ROM (Read-Only Memory)Stores the firmware or program that defines the device's functionality
- RAM (Random Access Memory)Provides temporary storage for variables and operational data
- EEPROM/Flash MemoryNon-volatile memory that can be electrically erased and reprogrammed
Input/Output (I/O) PortsAllow the microcontroller to interact with external components
Timers/CountersEnable precise timing operations and event counting
Communication InterfacesSuch as UART, SPI, I2C for connecting with other devices
Analog-to-Digital Converters (ADC)Convert analog signals to digital values for processing


The desktop computer you are using is a "general-purpose computer" that can run thousands of various programs. The microcontroller is a "dedicated computer" used for special purposes. It focuses on one thing. The microcontroller also has many common features. If a computer has most of the following characteristics, then you can call it a "microcontroller":

Microcontrollers are "embedded" in other devices to control the function and operation of the product. Therefore, the microcontroller is also called an "embedded controller". The microcontroller runs a specific program to complete a special task. This program is stored in ROM (Read Only Memory) and is generally not modified.

Microcontrollers are usually low-power devices. The power plug of a desktop computer is almost always plugged into a wall outlet, and its power is about 50 watts. The power of a battery-powered microcontroller is about 0.05 watts.

Microcontrollers have a dedicated input device, and usually (but not always) a light-emitting diode or LCD screen for output. The microcontroller also takes input signals from the devices it controls. It controls the device by sending signals to different parts of the device.

For example, a microcontroller in a television receives input signals from the remote control and displays them on the screen. The microcontroller will control the electronic adjustment of the channel selector, speakers, and some picture tubes. The engine controller in the car gets input signals from sensors such as oxygen and knock, and controls fuel mixing and spark plug timing. The microwave oven controller obtains the input signal from the operation keyboard, displays the output on the liquid crystal display, and controls the relay responsible for the microwave generator switch.

 

Block diagram of microcontroller

Block diagram of microcontroller

Microcontrollers are usually durable, but this is not always the case. For example, a microcontroller that controls a car's engine must be able to operate at a temperature limit that ordinary computers cannot withstand. The microcontroller of the car in Alaska, USA needs to work in the cold weather of minus 34 degrees Celsius, while the same controller needs to work in the hot environment of 49 degrees Celsius in Nevada. Coupled with the heat generated by the engine, the temperature of the engine box can be as high as 65-80 degrees Celsius.

The embedded microcontroller used inside the recorder does not have such requirements. There are many kinds of processors used as microcontrollers. For example, the Z-80 processor is an 8-bit microprocessor. It was born in the 1970s and was originally used in home computers at the time. The Garmin global positioning system in the working principle of the GPS receiver includes a low-power version of the Intel 80386 processor, which is said to be the case. The Intel 80386 processor was originally designed specifically for desktop computers.

In many products, such as microwave ovens, the performance requirements for microcontrollers are very low, and the price is the consumer’s main consideration. Under such circumstances, manufacturers began to design a dedicated microcontroller chip. It is an embedded central processor designed for low cost, small size, and low power consumption. Motorola 6811 and Intel 8051 are successful examples of such chips. There is also a series of controllers called "PIC microcontrollers" produced by Microchip. Judging by today's standards, these central processors are incredibly simple. However, the price for mass purchases is very low, and often only one piece can meet the needs of product designers.

 

Intel 8051 Pin Diagram

Intel 8051 Pin Diagram

A typical low-end microcontroller chip has about 1000 bytes of read-only memory and 20 bytes of random access memory, with 8 input and output pins. The unit cost of mass production of such chips is only a few cents. Of course, you can't expect to run programs like Microsoft Word on this chip because Microsoft Word requires about 30 megabytes of random access storage space and a processor that can execute millions of instructions per second. However, controlling a microwave oven does not require such a complicated program as Microsoft Word. What you want to accomplish with a microcontroller is a specific task. Low-cost and low-power operation is the most important.

Ⅱ Types of microcontroller

MCU is the abbreviation of the Microcontroller Unit. It is to appropriately reduce the frequency and specifications of the CPU. And interfaces such as memory, counter, USB, A/D conversion, UART, PLC, DMA, LCD driver circuits are integrated on a single chip to form a chip-level computer. The MCU can perform different combinations of control for different applications, such as mobile phones, PC peripherals, remote controllers, automotive electronics, industrial stepper motors, and robotic arms.

The MCU can be divided into without on-chip ROM type and with on-chip ROM type according to its memory type. For chips without on-chip ROM type, EPROM must be connected externally (typically 8031); chips with on-chip ROM type are divided into on-chip EPROM type (typical chip is 87C51) and MASK on-chip mask ROM type (typical The chip is 8051), on-chip Flash type (typical chip is 89C51) and other types.

Popular Microcontroller Families

  1. AVR (Atmel): Known for Arduino platforms

  2. PIC (Microchip): Widely used in industrial applications

  3. ARM Cortex-M Series: Dominating the 32-bit market

  4. ESP32/ESP8266: Popular for IoT applications

  5. STM32 (STMicroelectronics): Versatile 32-bit controllers

Microcontrollers can be divided into the general type and special type according to the use. According to the width of the data bus and the length of data bytes that can be processed at one time, it can be divided into 8, 16, 32-bit MCU.

Blew is the table showing difference types of microcontrollers:

CategoryTypeCharacteristics/Description
Based on Bit Width8-bit MicrocontrollersEconomical and power-efficient, suitable for simple applications with limited computing needs

16-bit MicrocontrollersOffer a balance between performance and power consumption

32-bit MicrocontrollersProvide higher processing power for complex applications requiring advanced computations

64-bit MicrocontrollersEmerging in high-performance embedded applications requiring extensive data handling
Based on Memory ArchitectureHarvard ArchitectureFeatures separate data and program memory buses, allowing simultaneous access

Von Neumann ArchitectureUses a single bus for both instructions and data, simplifying design but potentially limiting performance
Based on Instruction SetCISC (Complex Instruction Set Computing)Supports numerous complex instructions

RISC (Reduced Instruction Set Computing)Employs a simplified instruction set for efficient execution


Ⅲ What is the difference between a microcontroller and a microprocessor?

The controller is a single-chip microcomputer that integrates the main part of the microcomputer on one chip. The microcontroller was born in the mid-1970s. After more than 20 years of development, its cost is getting lower and lower, and its performance is becoming more and more powerful. Examples include motor control, barcode readers/scanners, consumer electronics, gaming equipment, telephones, HVAC, building security and access control, industrial control and automation, and white goods (washing machines, microwave ovens).

 

Microcomputer system structure

Microcomputer system structure

1 The role of the microcontroller

In industrial applications, the role of the microcontroller is to control and coordinate the activities of the entire device. It usually requires a program counter (PC), an instruction register (IR), an instruction decoder (ID), a timing and control circuit, and a pulse source.

According to the role played by the controller in the work, the microcontroller mainly has the following types:

1) Instruction controller

The instruction controller is a very important part of the controller. It must complete the operations such as fetching instructions and analyzing instructions and then hand it over to the execution unit (ALU or FPU) for execution. At the same time, it also forms the address of the next instruction.

2) Timing controller

The role of the timing controller is to provide control signals for each instruction in chronological order. The timing controller includes a clock generator and a frequency doubling definition unit. The clock generator sends out a very stable pulse signal from the quartz crystal oscillator, which is the main frequency of the CPU. The multiplier definition unit defines how many times the CPU's main frequency is the memory frequency (bus frequency).

3) Bus controller

The bus controller is mainly used to control the internal and external buses of the CPU, including the address bus, data bus, control bus, and so on.

4) Interrupt controller

The interrupt controller is used to control various interrupt requests. It queues the interrupt request according to the priority and hands it to the CPU for processing.

2 The basic functions of the device controller

As far as the control field is concerned, there are mainly the following functions:

1) Data buffer

The buffer is often built into the controller. During output, the buffer is used to temporarily store the data from the host at high speed, and then transfer the data in the buffer to the I / O device at the rate that the I / O device has. At input, the buffer is used to temporarily store the data sent from the I / O device. After receiving a batch of data, the data in the buffer is transferred to the host at high speed.

2) Error control

The device controller is also responsible for error detection of the data transmitted by the I / O device. If an error occurs during transmission, the error detection code is usually set and reported to the CPU, so the CPU discards the data transmitted this time and performs another transmission. In this way, the accuracy of data input can be guaranteed.

3) Data exchange

This refers to data exchange between the CPU and the controller, and between the controller and the device. For the former, the CPU writes data to the controller in parallel or reads data from the controller in parallel via the data bus. For the latter, the device inputs data to the controller or transfers it from the controller to the device. For this, the data register must be set in the controller.

4) Identify and report equipment status

The controller will write down the status of the device for the CPU to understand. For example, the CPU can only start the controller to read data from the device when the device is in the ready-to-send state. To this end, a status register should be set in the controller, with each bit in it to reflect a certain state of the device. When the CPU reads the contents of this register, it can understand the status of the device.

5) Receive and recognize commands

The CPU can send a variety of different commands to the controller, and the device controller should be able to receive and recognize these commands. To this end, there should be corresponding control registers in the controller to store the received commands and parameters and to decode the received commands. For example, the disk controller can receive 15 different commands such as Read, Write, and Format from the CPU, and some commands also have parameters. Accordingly, there are multiple registers and command decoders in the disk controller.

6) Address recognition

Just like every unit in memory has an address, every device in the system also has an address. The device controller must be able to recognize the address of every device it controls. Also, for the CPU to write (or read) data to (or from) registers, these registers should all have unique addresses. For example, in the IB-MPC machine, the address of each register in the hard disk controller is one of 320 ~ 32F. The controller should be able to correctly recognize these addresses. For this purpose, an address decoder should be configured in the controller.

3 The difference between a microprocessor and a microcontroller

This difference is mainly concentrated in three aspects: hardware structure, application field, and instruction set characteristics:

1) Hardware structure

The microprocessor is a single-chip CPU, and the microcontroller integrates the CPU and other circuits in an integrated circuit chip to form a complete microcomputer system. In addition to the CPU, the microcontroller also includes RAM, ROM, a serial interface, a parallel interface, a timer and interrupt scheduling circuit. These are integrated into an integrated circuit. Although the on-chip RAM has a smaller capacity than ordinary microcomputer systems, this does not limit the use of microcontrollers. It can be learned later that the application range of the microcontroller is very wide.

An important feature of the microcontroller is the built-in interrupt system. As a control-oriented device, microcontrollers often have to respond to external stimuli (interruptions) in real-time. The microcontroller must perform a fast context switch, suspend one process to execute another process in response to an "event". For example, opening a microwave oven door is an event. In a microcontroller-based product, this event will trigger an interrupt. The microprocessor can also have a powerful interrupt function, but usually requires the cooperation of external components, and the microcontroller integrates all the necessary circuits to handle interrupts on the chip.

2) Application areas

Microprocessors are usually used as CPUs in microcomputer systems. Its design is precisely for such applications, which is also the advantage of the microprocessor. However, microcontrollers are often used for control-oriented applications. The system design pursues miniaturization and minimizes the number of components. In the past, these applications usually required dozens or even hundreds of digital integrated circuits. The use of a microcontroller can reduce the number of components used. Only a microcontroller, a small number of external components, and control programs stored in ROM can achieve the same function. Microcontrollers are suitable for those occasions where very few components are used to control input/output devices. Microprocessors are suitable for information processing in computer systems.

3) Instruction set features

Due to different applications, the instruction sets of microcontrollers and microprocessors are also different. The microprocessor's instruction set enhances processing capabilities, giving it a powerful addressing mode and instructions suitable for operating large-scale data. The instructions of the microprocessor can operate on nibbles, bytes, words, and even double words. By using address pointers and address offsets, the microprocessor provides an addressing mode that can access large amounts of data. Self-increasing and self-decreasing modes make it very easy to access data in bytes, words, or double words. Besides, the microprocessor has other features, such as the inability to use privileged instructions in user programs.

The instruction set of the microcontroller is suitable for input/output control. Many input/output interfaces are a single bit. For example, the electromagnet controls the switch of the motor, and the electromagnet is controlled by a 1-bit output port. The microcontroller has instructions for setting and clearing units, and can also perform other bit-oriented operations, such as logical AND, OR, and XOR operations on "bits". Few microprocessors have these powerful bit manipulation capabilities, because designers only consider operating data in bytes or larger units when designing microprocessors.

In terms of device control and monitoring (perhaps through a 1-bit interface), the microcontroller has dedicated internal circuits and instructions for input/output, timing, and priority assignment of external interrupts. Microprocessors generally need to cooperate with additional circuits (serial interface chip, interrupt controller, timer, etc.) to perform the same task. However, in terms of processing power alone, the microcontroller will never reach the level of a microprocessor because a large part of the integrated circuit in the microcontroller chip is used to implement other on-chip functions.

Due to the very limited resources on the microcontroller chip, the instructions must be very streamlined, and most instructions are shorter than 1 byte in length. The design principle of the control program is usually that the program can be loaded into the on-chip ROM. This is because even adding only one external ROM will significantly increase the hardware cost of the product. The basic feature of the microcontroller instruction set is a streamlined coding scheme. Microprocessors do not have such characteristics, because their powerful addressing mode makes the instruction coding not simple enough.

Frequently Asked Questions

What are microcontrollers used for?

Microcontrollers (MCUs) are compact integrated circuits designed to manage specific tasks in electronics. They are used for various applications including:

  • Reading sensors 

  • Connecting devices over Wi-Fi 

  • Home automation and robotics 

  • Industrial IoT applications 

  • Wearable technology 

Everyday objects like cars, microwaves, fitness bands, thermostats, and even specialized projects like Arduino-powered coffee makers use microcontrollers.  Because of their adaptability, microcontrollers are crucial parts of the electronics industry, with several models tailored for particular uses.

Is a Raspberry Pi a microcontroller?

The typical Raspberry Pi is a single-board computer rather than a microcontroller.  Nonetheless, the Raspberry Pi Pico, one of the top IoT microcontrollers for 2025, is a product of the Raspberry Pi company.  Unlike the standard Raspberry Pi boards, which run full operating systems, the Raspberry Pi Pico is primarily made for microcontroller applications.

What is an example of a microcontroller?

Several examples of microcontrollers include:

  • ESP32: Known for its Wi-Fi capabilities and dual-core multitasking, making it great for connected robots 

  • STM32: Listed among the best IoT microcontrollers for 2025 

  • Teensy 4.1: Another top microcontroller option 

  • 8051: An older but still industrially relevant microcontroller with decades of use and robust community support 

Different microcontrollers are optimized for different purposes, such as power efficiency, connectivity options, or processing capabilities .

Is an Arduino a microcontroller?

Indeed, microcontrollers are what Arduino boards are.  In particular, the Arduino UNO is listed as one of the top IoT microcontrollers for 2025.  Popular for a wide range of uses, Arduino platforms are especially well-suited for novices while yet providing features for more seasoned developers.  For electronics projects, they are just one of many microcontroller possibilities accessible.

Conclusion

A key technological advancement that has completely changed the way electrical gadgets operate is the microcontroller.  They are perfect for the rising need for smart, connected devices because of their small size, energy economy, and specific functionality.  Microcontrollers will probably become even more potent, effective, and commonplace as technology develops, spurring industry innovation and opening up new uses in our globally interconnected society (Banzi & Shiloh, 2022).

References

Barrett, S. F., & Pack, D. J. (2021). Microcontrollers fundamentals for engineers and scientists (2nd ed.). Morgan & Claypool Publishers.

Banzi, M., & Shiloh, M. (2022). Getting started with Arduino (4th ed.). O'Reilly Media.

Heath, S. (2022). Embedded systems design (3rd ed.). Newnes.

Mazidi, M. A., Naimi, S., & Naimi, S. (2021). The AVR microcontroller and embedded systems: Using Assembly and C (3rd ed.). Pearson.

Toulson, R., & Wilmshurst, T. (2017). Fast and effective embedded systems design: Applying the ARM mbed (2nd ed.). Newnes.

Valvano, J. W. (2019). Introduction to ARM Cortex-M microcontrollers: Volume 1 (5th ed.). Self-published.

White, E. (2020). Making embedded systems: Design patterns for great software (2nd ed.). O'Reilly Media.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1 What is a microcontroller used for?

Microcontrollers are used in automatically controlled products and devices, such as automobile engine control systems, implantable medical devices, remote controls, office machines, appliances, power tools, toys, and other embedded systems.

2 What are examples of microcontrollers?

List of common microcontrollers:

Altera.

Analog Devices.

Atmel.

Cypress Semiconductor.

ELAN Microelectronics Corp.

EPSON Semiconductor.

Espressif Systems.

Freescale Semiconductor.

3 Is Arduino a microcontroller?

Most Arduino boards consist of an Atmel 8-bit AVR microcontroller (ATmega8, ATmega168, ATmega328, ATmega1280, or ATmega2560) with varying amounts of flash memory, pins, and features. Arduino microcontrollers are pre-programmed with a boot loader that simplifies uploading of programs to the on-chip flash memory.

4 What is the difference between Arduino and microcontroller?

The microcontroller is basically a Microprocessor having RAM, ROM, and I/O Ports. Arduino is an open-source hardware and software company that develops Arduino Boards. Arduino Boards are microcontroller development boards that consist of a Microcontroller as a part of it along with a USB port, GPIO pins, etc.

5 What are the disadvantages of microcontrollers?

There are some disadvantages of the microcontroller are given below,
The microcontroller cannot interface high power devices directly.

It has a more complex structure as compared to microprocessors.
It only performed a limited number of executions simultaneously.
It is generally used in micro equipment.
Related Articles

  • Getting Started with Arduino: What is Arduino and How to Use Arduino Boards
    Getting Started with Arduino: What is Arduino and How to Use Arduino Boards
    UTMEL28 September 20236268

    Arduino is an open-source electronics platform that includes software and programmable circuit boards, allowing beginners to build electronic projects by writing simple code. The article provides an overview of Arduino, including different board types, basic components, how to use the boards, and project ideas like an automated plant watering system.

    Read More
  • Arduino vs. Raspberry Pi: A Detailed Comparison
    Arduino vs. Raspberry Pi: A Detailed Comparison
    UTMEL24 April 20254979

    Hello everyone, welcome to the new post today.This guide is going to talk in detail about Arduino vs. Raspberry Pi to clarify their differences and help you pick the right board based on your needs.

    Read More
  • Electronic Components in the Smart Home System
    Electronic Components in the Smart Home System
    UTMEL24 April 20252478

    Electronic parts are the heart of every smart home system. These parts help devices talk, do tasks, and save energy. For instance, sensors notice motion or temperature changes. Microcontrollers use this data to do things like dim lights or turn on alarms.

    Read More
  • Software Tools for NXP Microcontroller Development
    Software Tools for NXP Microcontroller Development
    UTMEL06 June 20251278

    Discover how NXP microcontroller tools like MCUXpresso IDE, SDK, and Config Tools streamline coding, debugging, and hardware setup for embedded systems.

    Read More
  • VFD Driving Guide: What to Do When Your MCU Runs Out of Pins?
    VFD Driving Guide: What to Do When Your MCU Runs Out of Pins?
    UTMEL22 July 2025951

    This comprehensive guide addresses a common challenge faced by electronics enthusiasts: driving Vacuum Fluorescent Displays (VFDs) when microcontrollers have insufficient pins. Sparked by a Reddit user's question about controlling a VFD with more segments than available MCU pins, the article explores the elegant solution of multiplexing technology.

    Read More