Varistor: Definition, Function, Working and Testing

What is a Varistor?
Catalog
Ⅰ What is a varistor?
A varistor is a device with a non-linear volt-ampere characteristic. It is mainly used to clamp the voltage when the circuit is subjected to overvoltage and absorb excess current to protect sensitive devices. It is also called "Voltage-Dependent Resistor" abbreviated as "VDR". The material of the resistor body of a varistor is a semiconductor, so it is a variety of semiconductor resistors. The "zinc oxide" (ZnO) varistor, which is now widely used, has the main material composed of the divalent element zinc (Zn) and the hexavalent element oxygen (O). So from the perspective of materials, the zinc oxide varistor is a kind of "II-VI oxide semiconductor". When subjected to voltage below their threshold value, varistors act as high-resistance components, effectively blocking current flow. However, when voltage exceeds this threshold, they rapidly transition to a low-resistance state, diverting potentially damaging current away from sensitive components (Wang et al., 2019).
Varistors are semiconductor devices designed primarily to protect electronic circuits from voltage spikes and transients. The most widely used type is the Metal Oxide Varistor (MOV), typically composed of zinc oxide (ZnO) grains separated by grain boundaries that create semiconductor junctions (Nahm, 2020). From a materials science perspective, zinc oxide varistors belong to the II-VI oxide semiconductor family, combining the divalent element zinc (Zn) with the hexavalent element oxygen (O).
The non-linear resistance property makes varistors invaluable in circuit protection applications, where they can clamp transient voltages to safe levels before they reach sensitive components. This protective function is vital in various applications, from consumer electronics to industrial power systems (Pillai et al., 2021).

A varistor
A varistor is a voltage-limited protection device. Utilizing the non-linear characteristics of the varistor, when an overvoltage occurs between the two poles of the varistor, the varistor can clamp the voltage to a relatively fixed voltage value, thereby achieving protection of the subsequent circuit. The main parameters of the varistor are varistor voltage, current capacity, junction capacitance, response time, etc.
Ⅱ How do varistors work?
Varistors operate based on their distinctive voltage-dependent resistance characteristics:
Normal Operation Mode: When the applied voltage remains below the varistor's threshold value, it exhibits extremely high resistance (typically megaohms), allowing only negligible leakage current to flow. In this state, the varistor essentially functions as an open circuit.
Protection Mode: When voltage exceeds the threshold, the varistor's resistance dramatically decreases (by several orders of magnitude), allowing it to conduct significant current. This creates a low-impedance path that diverts the surge current away from protected components (Mahanty & Gupta, 2018).
The transition between these two states occurs with remarkable speed. Varistors typically respond to overvoltage events within nanoseconds, making them suitable for protecting against fast transients. While this response time is slower than Transient Voltage Suppressor (TVS) diodes, it is significantly faster than gas discharge tubes, offering an optimal balance for many applications (Ribeiro et al., 2021).
The response time of the varistor is ns level, which is faster than the gas discharge tube and slightly slower than the TVS tube. Generally, the response speed of overvoltage protection for electronic circuits can meet the requirements. The junction capacitance of a varistor is generally in the order of hundreds to thousands of Pf. In many cases, it should not be directly applied to the protection of high-frequency signal lines. When applied to the protection of AC circuits, the large junction capacitance will increase the leakage. The current needs to be fully considered when designing the protection circuit. The varistor has a larger flow capacity but is smaller than a gas discharge tube.
When the voltage applied to the varistor is lower than its threshold, the current flowing through it is extremely small, which is equivalent to a resistor with infinite resistance. That is when the voltage applied to it is below its threshold, it is equivalent to an off-state switch.

When the voltage applied to the varistor exceeds its threshold, the current flowing through it increases sharply, which is equivalent to an infinitely small resistance. In other words, when the voltage applied to it is higher than its threshold, it is equivalent to a closed state switch.
Ⅲ Main parameters of the varistor
The main parameters of the varistor are nominal voltage, voltage ratio, maximum control voltage, residual voltage ratio, current capacity, leakage current, voltage temperature coefficient, current temperature coefficient, voltage nonlinear coefficient, insulation resistance, static capacitance, etc..
1. The nominal voltage refers to the voltage value across the varistor when a 1mA DC is passed.
2. The voltage ratio refers to the ratio of the voltage value generated when the current of the varistor is 1 mA and the voltage value generated when the current of the varistor is 0.1 mA.
3. The maximum limiting voltage refers to the highest voltage value that the two ends of the varistor can withstand.
4. Residual voltage ratio: When the current flowing through the varistor is a certain value, the voltage generated across it is called this current value as the residual voltage. The residual voltage ratio is the ratio of the residual voltage to the nominal voltage.
5. The through-current capacity is also called the through-flow capacity, which refers to the maximum pulse (peak) current allowed to pass through the varistor under specified conditions (with a specified time interval and number of times, standard inrush current is applied).
6. Thw leakage current and waiting current refer to the current flowing through the varistor at the specified temperature and maximum DC voltage.
7. The voltage temperature coefficient refers to the rate of change of the nominal voltage of the varistor within a specified temperature range (temperature 20 ~ 70 °C), that is, when the current through the varistor remains constant, the relative change of both ends of the varistor when the temperature change 1 ℃.
8. The current temperature coefficient refers to the relative change in the current flowing through the varistor when the temperature across the varistor remains constant and the temperature changes by 1 °C.
9. The voltage non-linear coefficient refers to the ratio of static resistance value to the dynamic resistance value of a varistor under a given applied voltage.
10. The insulation resistance refers to the resistance value between the lead (pin) of the varistor and the insulating surface of the resistor body.
11. The static capacitance refers to the inherent capacitance of the varistor itself.
Ⅳ The function of varistors
Varistors serve several critical functions in electronic systems:
Transient Voltage Suppression: Their primary role is to suppress voltage spikes that could damage sensitive electronic components.
Lightning Protection: Especially in power distribution and telecommunications equipment, varistors provide protection against lightning-induced surges.
Switching Surge Suppression: They protect against high-voltage transients caused by switching operations in power systems.
Electrostatic Discharge (ESD) Protection: Varistors can help guard against damage from static electricity discharge.
Voltage Regulation: In some specialized applications, varistors assist in maintaining voltage within acceptable limits (Kumar et al., 2020).
The main function of the varistor is to protect the transient voltage in the circuit. Due to its working principle as described above, the varistor is equivalent to a switch. Only when the voltage is higher than its threshold, and the switch is closed, the current flowing through it surges and the impact on other circuits does not change much, thereby reducing the impact of overvoltage on subsequent sensitive circuits. This protection function of the varistor can be used repeatedly and can also be made into a one-time protection device similar to a current fuse.
The protection function of the varistor has been widely used. For example, the power circuit of a household color TV uses a varistor to complete the overvoltage protection function. When the voltage exceeds a threshold value, the varistor reflects its clamping characteristics. The excessive voltage is pulled low so that the subsequent circuit works within the safe voltage range.
The varistor is mainly used for transient overvoltage protection in a circuit, but because of its volt-ampere characteristics similar to a semiconductor Zener, it also has a variety of circuit element functions. For example, the varistor is a kind of DC high voltage small current-voltage stabilizing element with a stable voltage of thousands of volts or more, which cannot be reached by silicon Zener. Varistor can be used as a voltage fluctuation detection element, a DC level shifter Bit element, a fluorescent starting element, a voltage equalizing element, and so on.
Ⅴ Metal oxide varistor
The most common varistor is a metal oxide varistor (MOV), which contains a ceramic block composed of zinc oxide particles and a small number of other metal oxides or polymers, sandwiched between two metal sheets. A diode effect is formed at the junction of particles and adjacent oxides. Due to a large number of messy particles, it is equivalent to a large number of back-connected diodes. There is only a small reverse leakage current at low voltage. When high voltage is encountered, the diode reverse collapse occurs due to hot electrons and tunneling effect, and a large current flows. Therefore, the current-voltage characteristic curve of a varistor is highly non-linear: high resistance at low voltage and low resistance at high voltage.
The resulting microstructure features ZnO grains separated by grain boundaries that form semiconducting junctions. These junctions create the non-linear electrical properties that define MOV behavior. When voltage exceeds the threshold, these junctions break down in a controlled manner, allowing current to flow (Chen et al., 2019).
MOVs offer several advantages:
High energy absorption capability
Fast response time
Ability to handle repeated surge events
Relatively low cost and high reliability in appropriate applications
However, they also have limitations, including aging effects after repeated surges and potential catastrophic failure when subjected to surges beyond their rating (Wen & Wang, 2020).
Metal oxide varistors are currently the most common voltage clamping devices and can be used for various voltages and currents. The use of metal oxides in its structure means that MOVs are very effective in absorbing short-term voltage transients and have higher energy handling capabilities.
Like ordinary varistors, metal oxide varistors begin to conduct at a certain voltage and stop conducting when the voltage is lower than the threshold voltage. The main difference between the standard silicon carbide (SiC) varistor and the MOV type varistor is that the leakage current of the zinc oxide material through the MOV is very small under normal operating conditions, and its operating speed is much faster in the clamping transient.
MOVs usually have radial leads and a hard outer blue or black epoxy coating, which is very similar to disc ceramic capacitors and can be physically mounted on circuit boards and PCBs in a similar manner. The structure of a typical metal oxide varistor is as follows:

Metal oxide varistor structure
To select the correct MOV for a specific application, it is necessary to understand the source impedance and the possible pulse power of the transient. For input line or phase transients, the selection of the correct MOV is slightly more difficult, because the characteristics of the power supply are generally unknown. Generally speaking, the electrical protection of MOV selection circuit power transients and spikes is usually just an educated guess.
However, metal oxide varistors can be used for a variety of varistor voltages, from about 10 volts to more than 1000 volts AC or DC, so it can help you choose by knowing the supply voltage. For example, choose MOV or silicon varistor. For voltage, its maximum continuous root means square voltage rating should be slightly higher than the highest expected power supply voltage. For example, a 120-volt power supply is 130 volts rms, and 230 volts is a 260 volts rms supply.
The maximum surge current value that the varistor will use depends on the transient pulse width and the number of pulse repetitions. An assumption can be made about the width of the transient pulse, which is usually 20 to 50 microseconds (μs) long. If the peak pulse current rating is insufficient, the varistor may overheat and be damaged. Therefore, if the varistor operates without any failure or degradation, it must be able to quickly dissipate the absorbed energy of the transient pulse and safely return to its pre-pulse state.
Ⅵ Characteristics of a damaged varistor
A resistor is the most numerous component in electrical equipment, but it is not the component with the highest damage rate. An open circuit is the most common type of resistance damage. It is rare for resistance to become large, and it is very rare for resistance to become small. Common types are carbon film resistors, metal film resistors, wire wound resistors, and fuse resistors. The first two types of resistors are the most widely used. Their damage characteristics are low resistance (below 100Ω;) and high resistance (above 100Ω;). The second is that when the low resistance resistor is damaged, it is often burnt and blackened, which is easy to find, and when the high resistance resistor is damaged, there are few traces. Wire-wound resistors are generally used for high current limiting, and the resistance is not large. When the cylindrical wire-wound resistor is burned out, some of it will become black or the surface will explode, crack. Cement resistance is a kind of wire wound resistance, which may break when burned out, otherwise, there will be no visible traces. When the fuse is burnt out, some surfaces will blast off, and some will have no trace, but they will never burn and become black.
Ⅶ How to test varistors?
1. Preparation before varistor measurement
Connect the two test leads (regardless of positive and negative) to the two ends of the resistor to measure the actual resistance value. To improve the measurement accuracy, the range is selected according to the nominal value of the measured resistance. Due to the non-linear relationship of the ohm scale, the middle section of the scale is fine. Therefore, the pointer value should fall as far as possible to the middle of the scale, that is, within the range of 20% to 80% of the radian of the full scale. According to the resistance error level, an error of ± 5%, ± 10%, or ± 20% is allowed between the reading and the nominal resistance, respectively. If the error range is exceeded, the resistor has changed the standard value.
2. How to measure the quality of a varistor?
Judging the varistor usually requires a power supply with a wide regulating voltage range, and it has a good current limiting effect. A voltmeter with good precision is connected in parallel across the varistor when measuring. Connect the adjustable power lead to both ends of the varistor.
The voltmeter indicates the power supply voltage. You should slowly adjust the voltage and will observe that the voltage suddenly drops after reaching a certain voltage. The voltage at the last moment before the decrease is the protection value of the varistor.
With the continuous voltage applied to the varistor, its resistance value can change from MΩ (Megohm) to mΩ (Milliohm). When the voltage is low, the varistor works in the leakage current region, showing a large resistance, and the leakage current is small; when the voltage rises into the non-linear region, the current changes within a relatively large range, and the voltage does not change much showing a good voltage limiting characteristic; when the voltage is raised again, the varistor enters the saturation region and presents a very small linear resistance. Due to the large current, the varistor will overheat and burn or even burst over time.

A multimeter
3. Selection of varistor
When selecting a varistor, the specific conditions of the circuit must be considered, and generally, the following principles should be followed:
(1) Selection of varistor voltage V1mA
According to the selection of the power supply voltage, the power supply voltage continuously applied across the varistor must not exceed the "maximum continuous operating voltage" value listed in the specification. That is, the maximum DC operating voltage of the varistor must be greater than the DC operating voltage VIN of the power line (signal line), that is, VDC ≥ VIN; For the selection of the 220V AC power source, the fluctuation range of the operating voltage of the power grid must be fully considered. The general fluctuation range of the domestic power grid is 25%. A varistor with a varistor voltage of 470V to 620V should be selected. Selecting a varistor with a higher varistor voltage can reduce the failure rate and prolong the service life, but the residual voltage is slightly increased.
(2) Selection of traffic
The nominal discharge current of the varistor should be greater than the surge current required to withstand or the maximum surge current that may occur during equipment operation. The nominal discharge current should be calculated by pressing the value of more than 10 shocks in the rating curve of times of the surging life, which is about 30% of the maximum shock flux (ie, 0.3IP).
(3) Selection of clamping voltage
The clamping voltage of the varistor must be less than the maximum voltage (ie, safe voltage) that the component or equipment being protected can withstand.
(4) The choice of capacitor Cp
For high-frequency transmission signals, the capacitance Cp should be smaller, and vice versa
(5) Internal resistance matching (Resistance Match)
The relationship between the internal resistance R (R≥2Ω) of the protected component (line) and the transient internal resistance Rv of the varistor: R≥5Rv; for the protected component with small internal resistance, without affecting the signal transmission rate, you should try to use a large capacitor varistor.
Conclusion
Varistors represent a critical component in the protection of electronic circuits against overvoltage events. Their unique non-linear resistance properties enable them to effectively safeguard sensitive components from transient voltage spikes that could otherwise cause catastrophic failure. By understanding the fundamental principles, key parameters, and proper testing methods for varistors, engineers can implement robust protection strategies for electronic systems across diverse applications.
As power electronics continue to advance and electronic devices become increasingly compact and sensitive, the role of varistors in circuit protection remains essential. Ongoing developments in varistor technology, including new material compositions and manufacturing techniques, continue to enhance their performance characteristics and reliability.
References
Chen, L., He, X., & Wu, K. (2019). Microstructure and electrical properties of ZnO-based varistors with different additives. Journal of Materials Science: Materials in Electronics, 30(5), 5107-5115. https://doi.org/10.1007/s10854-019-00911-2
He, J., & Hu, J. (2022). Temperature dependency of modern metal oxide varistors and its impact on surge protection applications. IEEE Transactions on Power Delivery, 37(1), 471-479. https://doi.org/10.1109/TPWRD.2021.3068046
Kumar, A., Singh, R., & Sharma, V. (2020). Varistor technology and its application in modern protection systems: A comprehensive review. Electrical Engineering, 102(1), 83-105. https://doi.org/10.1007/s00202-019-00871-0
Luo, F., Wang, Z., & Lu, Y. (2018). Failure analysis and diagnosis of metal oxide varistors under multiple lightning strikes. IEEE Transactions on Power Delivery, 33(5), 2327-2335. https://doi.org/10.1109/TPWRD.2018.2797248
Mahanty, R., & Gupta, A. (2018). Surge protection devices for electronic equipment: Principles, applications, and selection criteria. IEEE Electrical Insulation Magazine, 34(5), 8-20. https://doi.org/10.1109/MEI.2018.8507714
Nahm, C. W. (2020). Zinc oxide varistors with improved nonlinear properties and energy absorption capabilities. Journal of Materials Science: Materials in Electronics, 31(4), 2932-2942. https://doi.org/10.1007/s10854-019-02837-1
Related Articles:
SMD Resistors: Codes, Size, Testing, Tolerance and Selection
What are the Differences Between Pull up and Pull down Resistors?
1.What is a varistor used for?
Varistors are used to protect a circuit from high voltage surges. When a high voltage surge is applied to a circuit, the outcome is usually catastrophic to the circuit. A capacitor may be installed across the signal lines.
2.What happens when a varistor fails?
Because the varistor has a negative temperature coefficient, the current will increase as the varistor becomes hotter. Thermal runaway may occur, with consequent failure of the varistor.
3.How do you test for varistor?
Touch one meter probe to the free varistor lead and the other probe to the connected lead. Read the resistance on the meter. If it reads nearly infinite resistance, the varistor is still good. If it reads very low resistance, the varistor is blown.
4.Do varistors have polarity?
Metal Oxide Varistors are similar to resistors and has only two leads. There is no polarity for these leads and hence can be connected in both directions.
5.Why would a varistor burn out?
When the varistor leakage current is too large, and the temperature rises to a certain extent, the low melting point metal is melted, thereby varistor from The cutting in the circuit can effectively prevent the varistor from burning.
What are the Differences Between Pull up and Pull down Resistors?UTMEL22 October 202537109Pull up is to clamp an uncertain signal to a high level with a resistor, and the resistor also acts as a current limiter. In the same way, pull down means to clamp the uncertain signal to a low level through a resistor. To pull up is to input current to the device, and the pull-down is to output the current.
Read More
Rheostat Basics: Types, Principle and FunctionsUTMEL25 December 202516951A rheostat is a device that can adjust the size of the resistance and can be connected to the circuit to adjust the size of the current. A general rheostat is composed of a wire with a larger resistance and a device that can change the contact point to adjust the effective length of the resistance wire. Rheostat can limit the current and protect the circuit, and change the voltage distribution in the circuit.
Read More
Basic Introduction to Metal Film ResistorUTMEL28 August 202013252Metal film resistors are a kind of film resistors. Metal film resistors are resistors in which special metals or alloys are used as resistor materials, and the resistor film layer is basically formed on ceramic or glass by vacuum evaporation or sputtering.
Read More
Varistor: Definition, Function, Working and TestingUTMEL03 April 202582277A varistor is a device with a non-linear volt-ampere characteristic. When the voltage applied to the varistor is lower than its threshold value, the current flowing through it is extremely small, which is equivalent to a resistor with infinite resistance, vice versa. The most common varistor is a metal oxide varistor (MOV).
Read More
Photoresistor Basics: Types, Principles and ApplicationsUTMEL16 October 202544057The article introduces the photoresistor’s main characteristics and principles including the working principle and structural principle. There are three types of photoresistor: ultraviolet photoresistors, infrared photoresistors, visible light photoresistors. Dimming circuit and light switch are the two applications of the photoresistor.
Read More
Subscribe to Utmel !
BGA614H6327XTSA1Infineon Technologies
AD8351ARMZAnalog Devices Inc.
AD8346ARUZAnalog Devices Inc.
ADL5531ACPZ-R7Analog Devices Inc.
BGA725L6E6327FTSA1Infineon Technologies
AD8361ARTZ-RL7Analog Devices Inc.
TDA5235XUMA1Infineon Technologies
ADL5511ACPZ-R7Analog Devices Inc.
AD8318ACPZ-REEL7Analog Devices Inc.
LMX2582RHARTexas Instruments


Product
Brand
Articles
Tools