13 kinds of sensors in mobile phones and what are recorded by the sensors

What Sensors Are in a Smartphone?
Summary: Modern smartphones rely on a complex array of built-in sensors—such as accelerometers, gyroscopes, and ambient light sensors—to interact with the physical world. The global smartphone sensors market is projected to reach $92.75 billion by 2033, driving innovations in augmented reality, biometric security, and health tracking. Understanding how these components function is essential for maximizing device utility and protecting personal privacy.
Topics covered in this article:
Ⅰ. What is a cell phone sensor?
A mobile phone sensor is a micro-electromechanical component within a device designed to detect physical environmental changes—such as motion, light, and pressure—and convert them into digital data. It detects changes in the environment or the state of the phone itself, measuring physical quantities such as distance, light, temperature, gravity, and pressure.
Just like other electronic components (CPUs, memory), sensors are following the trend of Moore's Law. The global smartphone sensors market is projected to reach $92.75 billion by 2033, growing at an 8.0% CAGR as components become progressively smaller and more powerful.
The mobile phone's operating system and software analyze the raw data acquired by these sensors to power numerous applications. Today's smartphones leverage these sensors to make social networking, financial transactions, fitness tracking, augmented reality gaming, and learning extremely convenient.
Ⅱ. What sensors are there in smartphones?
Modern smartphones typically contain over a dozen built-in sensors, categorized primarily into motion, environmental, positional, and biometric sensors. In the past, sensors were strictly used for physical measurement. Today, they convert those measurements into complex data streams used by intelligent algorithms. The smartphone sensor market is expected to grow by 12% annually, driving rapid evolution in sensor fusion technology.
The type and number of embedded sensors in a smartphone are often dictated by the phone's tier (budget vs. flagship). However, almost all modern phones include the basics linked to movement. The following are examples of common mobile phone sensors:
1. Accelerometer

An accelerometer is a motion sensor that measures the acceleration forces of a smartphone in three dimensions (x, y, and z axes) to detect changes in velocity and orientation. Although the concepts of an acceleration sensor and a gravity sensor are often conflated, they have distinct functions. It primarily detects changes in velocity (speeding up or slowing down).
For example, when a user holds the phone and swings it, the sensor records the acceleration and detects the change in direction. Common applications include:
Pedometer functions: By analyzing the frequency and intensity of these swings (movements), the phone can calculate steps.
Gesture controls: This sensor is also used to trigger unique commands in games or everyday utilities, such as "shake to undo" or flipping the phone to mute a call.
Note: While energy-efficient, standard accelerometers have lower precision compared to gyroscopes, which is why they are often used in tandem.
2. G-Sensor (Gravity Sensor)

A G-sensor, or gravity sensor, specifically measures the directional force of gravity to determine the device's absolute orientation relative to the ground. Often implemented using piezoelectric effects or MEMS technology, it contains a mass that responds to gravity, allowing the phone to determine which way is "down."
Its most common application is Auto-Rotate: switching the screen from portrait to landscape mode when you turn the phone sideways. In gaming, it allows for steering in racing games by tilting the device.
3. Ambient Light Sensor

An ambient light sensor detects the intensity of surrounding light and automatically adjusts the smartphone's screen brightness to optimize visibility and conserve battery. Similar to how the human pupil constricts in bright light, this sensor acts as the "eyes" of the smartphone regarding brightness.
Since the display is typically the most power-hungry component of a smartphone, using this sensor to dim the screen in dark rooms can reduce display power consumption by up to 15%. It also helps prevent accidental touches when the phone is in a pocket (often working with the proximity sensor).
4. Proximity Sensor

A proximity sensor detects the presence of nearby objects without physical contact, typically using an infrared LED and detector to turn off the screen during phone calls. Usually located near the earpiece (or under the display in newer flagship phones), this sensor consists of an infrared LED and an infrared light detector.
When you hold the phone up to your ear during a call, the sensor detects the reflection of the invisible infrared light off your skin. It then instantly turns off the display. This serves two purposes: it saves battery power and prevents your ear/cheek from accidentally hanging up the call or pressing buttons (misoperation).
5. Magnetometer (Digital Compass)

A magnetometer measures the strength and direction of magnetic fields, functioning as a digital compass to determine the smartphone's orientation relative to magnetic North. This allows the phone to determine its orientation relative to North, South, East, and West.
It is critical for map applications (like Google Maps or Apple Maps) to show which direction you are facing. Without it, the map would know your location (via GPS) but not your orientation.
6. Gyroscope

A gyroscope measures angular velocity and rotation around an axis, allowing the smartphone to track complex 3D motion with high precision. While the accelerometer measures linear motion, the gyroscope measures rotation.
By combining data from the accelerometer and the gyroscope, system designers can track motion in 3D space with high precision. This is essential for:
Augmented Reality (AR): Keeping virtual objects anchored to the real world.
Photography: Optical Image Stabilization (OIS) and Electronic Image Stabilization (EIS) use gyros to counteract hand shake.
Gaming: Precise motion control (e.g., aiming a bow in a game by moving the phone).
7. GPS / GNSS Sensor

A GPS or GNSS sensor receives timestamped signals from orbiting satellites to calculate the smartphone's exact geographical coordinates for navigation and location tracking. While early systems relied on 24 US satellites, modern phones use GNSS (Global Navigation Satellite Systems). This connects not just to GPS (USA), but also Galileo (Europe), GLONASS (Russia), and BeiDou (China), utilizing dozens of satellites simultaneously for faster and more accurate positioning.
The GPS module receives timestamped signals from orbiting satellites. By calculating the time difference between signal transmission and reception from multiple satellites, the phone calculates its exact coordinates (trilateration). This is used for navigation, geotagging photos, and speed measurement.
8. Fingerprint Sensor

A fingerprint sensor is a biometric security component that scans the unique ridges of a user's finger to authenticate identity and unlock the device. Fingerprint sensors have evolved significantly:
Capacitive: Uses the finger as part of a capacitor array. The ridges and valleys of the print change the capacitance. (Often found on power buttons or back of phones).
Optical (Under-Display): Uses light to take a photo of the fingerprint through the screen (common in mid-range to high-end phones).
Ultrasonic (Under-Display): Uses sound waves to map the 3D ridges of the finger. It is more secure and works even with wet or oily fingers (found in premium devices like the Samsung Galaxy S series).
9. Hall Sensor

A Hall sensor detects the presence and strength of a magnetic field, primarily used in smartphones to recognize when a magnetic smart cover is opened or closed. Using the Hall Effect, its primary use in smartphones is for "smart flip covers." When a cover with a small magnet is closed over the screen, the Hall sensor detects the magnet and tells the phone to lock the screen or display a specialized clock interface through a window in the case.
10. Barometer
A barometer measures atmospheric pressure to calculate the smartphone's altitude, improving GPS accuracy and enabling fitness apps to track elevation changes. Since air pressure decreases as you go higher, this sensor allows the phone to calculate altitude. This helps GPS lock onto your location faster (providing the Z-axis or vertical height) and improves accuracy to within a few meters.
Health apps also use this data to count how many "flights of stairs" you have climbed during the day.
11. Heart Rate Sensor

A heart rate sensor uses Photoplethysmography (PPG) to measure pulse by detecting changes in light absorption as blood pumps through capillaries. Note: Dedicated heart rate sensors on the back of phones (like older Samsung Galaxy S5-S10 models) have become rare.
A high-brightness LED illuminates the capillaries in the finger, and a sensor detects the change in light absorption as blood pumps through. Today, this function has largely moved to smartwatches and fitness bands, though some apps can approximate this using the phone's main camera and flash.
12. Blood Oxygen (SpO2) Sensor
A blood oxygen sensor uses red and infrared light to measure the oxygen saturation of hemoglobin, though this feature is now more common in smartwatches than smartphones. While rare on phones now, it is a standard feature on almost all modern smartwatches for health tracking.
13. Temperature Sensor
A temperature sensor monitors the internal heat of the smartphone's battery and CPU to prevent overheating, while some modern devices include external sensors for measuring object temperatures. All smartphones have internal thermistors to monitor the battery and CPU temperature to prevent overheating.
2026 Update: While internal thermistors remain standard, devices like the Google Pixel 9 Pro and newer flagship models feature dedicated external temperature sensors. These allow users to measure the temperature of objects (like coffee or baby formula) and, with regulatory approval, human body temperature.
Sensor Comparison Overview
| Sensor Type | Primary Function | Common Application |
|---|---|---|
| Accelerometer | Measures linear acceleration | Step counting, screen rotation |
| Gyroscope | Measures angular rotation | 3D gaming, optical image stabilization |
| Magnetometer | Detects magnetic fields | Digital compass, map orientation |
| Ambient Light | Detects surrounding light intensity | Auto-brightness adjustment |
| Barometer | Measures atmospheric pressure | Altitude tracking, GPS enhancement |
Ⅲ. What Data Do Smartphone Sensors Record?
Smartphone sensors continuously record a vast array of personal data, including precise location, physical movement patterns, and audio-visual environmental cues. Your phone is a data collection powerhouse, and the combination of these sensors creates a "digital fingerprint" of your daily life.
Location & Movement: By combining GPS, Wi-Fi triangulation, and the accelerometer, apps can track not just where you are, but how you got there. They know if you are driving, walking, or running. Over a year, this creates a detailed heatmap of your life.
Audio & Voice: Microphones are sensors too. With the rise of "Always-on" assistants (Siri, Google Assistant), phones are constantly listening for wake words. While companies state this data is processed locally, concerns remain about inadvertent recordings.
Privacy Indicators: In response to these concerns, modern mobile operating systems (such as iOS 18+ and Android 15+) display a Green Dot (camera) or Orange Dot (microphone) in the status bar whenever an app is actively using these sensors.
Ⅳ. How Can You Protect Your Sensor Privacy?
You can protect your sensor privacy by regularly auditing app permissions, restricting location access to "only while using," and disabling unnecessary background data collection. As sensors get smaller and cheaper, the potential for surveillance increases. Unlike the days of removing a battery to "go dark," modern phones are sealed units.
However, panic isn't the solution—awareness is. Most data collection is for commercial profiling (ads), not malicious stalking. But commercial data can still be sold or leaked.
How to protect yourself:
Audit Permissions: Go to your Settings > Privacy > Permission Manager. Does a flashlight app really need your Location? Does a calculator need your Contacts? If yes, deny it or uninstall it.
"While Using" vs. "Always": When an app asks for location, choose "Only while using the app." Never grant "Always Allow" unless absolutely necessary (e.g., for a safety tracker).
Precise vs. Approximate Location: Newer operating systems allow you to give apps an "Approximate" location (good for weather apps) rather than "Precise" location (needed for navigation).
Ⅴ. What Are the Emerging Sensor Technologies in 2026?
Emerging smartphone sensor technologies in 2026 include advanced LiDAR for 3D mapping, Ultra-Wideband (UWB) for precise spatial awareness, and AI-driven sensor fusion for computational photography. Since the original publication of this article, several high-tech sensors have become standard in flagship devices:
LiDAR (Light Detection and Ranging): Found in "Pro" model iPhones and iPads, LiDAR shoots out lasers to create a precise 3D map of the room instantly. It drastically improves low-light autofocus in cameras and enables high-quality Augmented Reality (AR) experiences.
ToF (Time of Flight) 3D Cameras: Similar to LiDAR, these sensors measure depth, allowing for better portrait mode photos (background blur) and secure facial recognition.
UWB (Ultra-Wideband): A short-range communication sensor that provides spatial awareness. It allows your phone to act as a precise digital car key, find lost items (like AirTags) with directional accuracy, and transfer files by pointing your phone at another device.
Flicker Sensors: These detect the frequency of artificial lights (like fluorescent bulbs) to adjust the camera's shutter speed, preventing the "banding" effect in photos and videos.
Frequently Asked Questions
Can smartphone sensors be hacked?
Yes, malicious apps can potentially exploit smartphone sensors to gather sensitive data. Cybercriminals can use motion sensors like accelerometers and gyroscopes to infer keystrokes or PINs. To prevent this, always download apps from trusted stores and regularly review your device's permission settings.
Which sensor is used for auto-rotation in mobile?
Auto-rotation primarily relies on the accelerometer, which measures linear acceleration and detects the device's orientation relative to gravity. In more advanced applications, the gyroscope provides additional rotational data to ensure the screen transitions smoothly between portrait and landscape modes.
Do smartphone sensors drain battery?
While sensors do consume power, their impact is generally minimal due to low-power micro-electromechanical systems (MEMS) technology. In fact, sensors like the ambient light sensor and proximity sensor actively save battery life by automatically dimming or turning off the display when it is not needed.
1. What is the role of mobile phone sensors?
Mobile phone sensors can also identify which sensors the mobile phone hardware supports, and provide sensing tools that play an important role in our daily lives.
2. How to know if the phone's proximity sensor is broken?
During a call, cover the distance sensor on the upper part of the phone with your hand. If the screen is off, it proves to be good, if it is not off, it may be bad, because it depends on whether the distance sensor is set in the settings of the phone.
3. What is the principle of mobile phone distance sensor?
Generally consists of two components. One emits infrared rays, and the other detects and receives infrared rays. The two are placed at an angle. When the object is close enough, the object under test will reflect the infrared light to the component that receives or detects the infrared light. You can try to get a mirror. Place it a little farther away, and then adjust the angle. When the mirror reflects infrared rays to the receiver. The distance sensor will also falsely report. Also, human skin can scatter light, just like holding a flashlight and covering it with your hand, the whole hand will shine. At this time, the infrared detector can also sense infrared. Similarly, if you hold an opaque object against the proximity sensor, it will not respond. Because infrared rays cannot be detected.
The Key Role of Electronic Components in IoT DevicesUTMEL01 September 20235192The article discusses the pivotal role of electronic components in Internet of Things (IoT) devices. IoT devices work by capturing real-world data using sensors, processing it through a microcontroller, and then sending it to the cloud for further analysis.
Read More
How to Identify the Perfect Proximity Sensor for Your ApplicationUTMEL19 July 20251101Find the best proximity sensors for your project by evaluating material, sensing range, environment, and system needs to ensure optimal performance and reliability.
Read More
Trusted Vibration Sensors for Homeowners and Industry ProfessionalsUTMEL17 July 2025810Compare top vibration sensors for home and industrial use. Find trusted options for security, predictive maintenance, and equipment protection.
Read More
Wiring and Mounting Photoelectric Sensors in 2025UTMEL15 July 20251000Wire and mount photoelectric sensors in 2025 with step-by-step safety, wiring, and alignment tips for reliable installation and optimal sensor performance.
Read More
Essential Tips for Picking the Best Gas SensorUTMEL15 July 20252225Find out how to select gas sensors by matching target gases, environment, and compliance needs for reliable and accurate gas detection in any setting.
Read More
Subscribe to Utmel !
T0054470699Apex Tool Group
T0054451999Apex Tool Group
T0054449499Apex Tool Group
ETB-5Apex Tool Group
UMMYA-0750-1500-1Omron Automation and Safety
38-855Apex Tool Group
3872-3API Delevan
EBM60TZ220Menda
EPM80CP303Menda
50712Elesa USA Corporation


Product
Brand
Articles
Tools