The Evolution History of Storage Devices

Published: 06 October 2021 | Last Updated: 26 November 202565582
Some people say that "most technology products are destined to be open for only a short period of time." Today, I intend to talk about the evolutionary history of storage devices in the age of technology.
Learn about secondary or external memory or storage devices of a computer. It explains Magnetic, Optical, and Flash storage devices

Storage Devices

Topics covered in this post:

Storage Devices in the past

Storage devices commonly used today

New storage technologies looking to the future

Storage Devices in the past

After the changes in storage media such as knotted notes, oracle bones, stone tablets, paper, etc., the rise of the industrial revolution has also brought about the evolution of storage devices. The following will introduce the mechanical storage devices that emerged from the industrial age.

the development history of storage devices.png

Punched cards and punched paper tapes--the original storage form of mechanized information

In 1890, the American statistician Herman Hollerith invented the punch-card tabulating machine that can record up to 960 bits for collecting and counting census data. It marks the beginning of the era of semi-automatic data processing systems. It has gradually been widely used in the fields of industrial retrieval and data statistics.

Punched paper tape-sequence control principle.jpg

Punched paper tape-sequence control principle

Punched cards and punched paper tapes are used in punch card tabulation machines as input and output devices of early computers. It converts programs and data into binary codes, where holes are 1 and non-holes are 0, and then input into the computer through photoelectric scanning.

Magnetic tape-the beginning of the era of magnetic storage

In 1928, Fritz Pfleumer, an engineer from Dresno, Germany, invented the audiotape, which can store analog signals. The working principle of the magnetic tape is: the crushed magnetic particles are glued to the paper strip to prepare the magnetic tape. However, due to the fragile paper strips, audiotapes were not practical at that time. In 1951, magnetic tapes began to be used for computer data storage. One magnetic tape could replace 10,000 punched paper cards. In 1980, a small cassette tape appeared. A 90-minute tape can record approximately 660KB of data on each side. Today, advanced tape technologies like **LTO (Linear Tape-Open)** are still crucial in enterprise environments for **cost-effective, high-capacity long-term archival storage** and disaster recovery.

magnetic tape.jpg

magnetic tape

Drum memory-the predecessor of hard drives

In 1932, Gustav Tauschek, an Austrian engineer from IBM, invented the drum memory, which is 16 inches long. With 40 tracks, it can rotate 12,500 revolutions per minute, and can only store 10KB of data. Before the appearance of magnetic core memory, it was widely used in computer memory and was considered the predecessor of hard disk drives. The advantages of the magnetic drum are practical, reliable, economical, and the biggest disadvantage is that the storage capacity is too small and the utilization rate is low.

Drum memory.jpg

Drum memory

Magnetic core memory-an early version of random access memory (RAM)

In 1949, Dr. An Wang from the Harvard University Laboratory in the United States realized the "read and write" technology for magnetic core memory. The principle of magnetic core memory is that the magnetic core can produce two opposite directions of magnetization according to the direction of current during magnetization, and use this as a state of 0 and 1 to record data. The original magnetic core memory only had a capacity of a few hundred bytes. Magnetic core memory was widely used as the main memory of computers in the 1970s until Intel’s semiconductor DRAM memory was mass-produced.

Magnetic core memory.jpg

Magnetic core memory

Hard Disk Drive-Disk Storage Era

In 1956, IBM's Reynold B. Johnson led the R&D team to invent the world's first hard drive, the IBM 305 RAMAC. The drive is about the size of two refrigerators, weighs a ton. It contains 50 24-inch platters, has a capacity of only 5MB, and has a data transfer speed of 10K/S. Nowadays, desktop hard drives are generally 3.5 inches in size, and products with a capacity of **24TB or higher** have also been born, showcasing the continued evolution of magnetic storage density.

Hard Disk Drive.jpg

Hard Disk Drive

Floppy Disk--The earliest removable medium used in personal computers

In 1971, floppy disks were introduced by IBM and were widely used from the mid-1970s to the late 1990s. Initially, they were 8-inch disks, followed by 5.25-inch and 3.5-inch disks. The earliest read-only floppy disk had a capacity of 79.9KB in 1971, and a readable and writable version appeared one year later. Floppy disks are slow in access speed and small in capacity, but they are detachable and easy to carry.

3.5 inch floppy disk structure.jpg

3.5-inch floppy disk structure

CD-ROM-the storage carrier of optical information

In 1982, Sony and Philips released CDP-101, the world's first commercial CD audio player, and CD became popular. Early CDs were only used in the film industry, with a diameter of 30cm. Each side could record 60 minutes of video or audio. Nowadays, the storage density of CD technology has been continuously improved, and CD-ROM, DVD, D9, D18, and Blu-ray technology have appeared. Game discs of game consoles, retail movies, and materials that need to be stored for a long time can still be seen on the CD.

CD.jpg

CD


Storage devices commonly used today

With the development of computers, the Internet age is gradually coming. People's demand for information storage continues to increase, which also promotes the accelerated evolution of storage devices. Next, let's take a look at the storage devices that are commonly used today.

Solid State Drive-Simplified Computer System

In 1989, the first solid-state hard drive appeared, also known as a solid-state drive, which was a hard drive made of an array of solid-state electronic memory chips. Since then, solid-state drives have gradually developed marketization and have been used in professional fields such as medical, aviation, and military fields. Compared with traditional hard disks, it has the advantages of fast read and write speed, shock and drop resistance, low power consumption, no noise, and lightness. Today, the shift to **NVMe (Non-Volatile Memory Express)** over the **PCIe bus** has dramatically increased performance beyond older SATA limits. There is still a life limit due to the limitation of the number of erasing and writing, though technologies like **TLC (Triple-Level Cell)** and **QLC (Quad-Level Cell)** are continually improving cost-efficiency and endurance.

Solid State Drive.jpg

Solid State Drive

SD card-a memory card based on semiconductor flash technology

In 1999, Japan's Panasonic, Toshiba, and SanDisk Corporation jointly developed an SD card. Initially, the capacity was only 2/4/8 MB, and it has now reached 128/512 GB or even 1T in the continuous update of the standard. In the era when mobile phones were only used for communication and MP4 was popular, SD cards became the main force for mobile data loading. Mobile phones were packed with more songs to act as a music player, and MP4 could download more movies to act as a small TV. The newest standards, such as **SD Express**, are introducing higher-speed data transfer that leverages the NVMe interface, making them suitable for demanding applications like professional **4K and 8K video recording**.

SD card.jpg

SD card

USB flash drive-a storage device using flash memory chips as storage media

In 1998, the USB flash drive was launched for the first time. In 2004, China Netac Technology Co., Ltd. obtained a basic invention patent for flash drives officially authorized by the US National Patent Office. It is characterized by "small size, large capacity." Just plug and unplug, the files in the computer can be packed and taken away at any time. Current standards like **USB 3.2** and **USB4/Thunderbolt 4** provide extremely fast data transfer speeds, and capacities routinely reach **2TB**, making them versatile tools. Bootable USB flash drives, anti-virus USB flash drives, temperature measurement USB flash drives, and music USB flash drives are also constantly being developed.

USB flash drive.jpg

USB flash drive


New storage technologies looking to the future

With the rapid development of cloud computing, big data, the Internet of Things, and artificial intelligence, people are also ushering in the era of "information explosion." Information has exploded, and storage is accelerating. It is believed that with the continuous advancement of technology, storage devices, as carriers of information, will also develop faster. Let's talk about the storage technology of the future.

Nano storage-a major direction for possible future development

In 1998, the University of Minnesota and Princeton University in the United States successfully developed a quantum disk, a nanoarray system composed of magnetic nanorods. A quantum disk is equivalent to our current 100,000 to 1 million disks, while energy consumption has been reduced by 10,000 times.

In 2002, a scientific research team from the University of Wisconsin in the United States developed an atomic-level silicon memory material whose density of information stored was 1 million times that of the current optical disk.

In 2014, Professor Sharon Grotz of the University of Michigan discovered in a study that the combination of nanoparticles is like a Rubik's Cube, twisting around a central point, and its state change can be used to encode information like a string of 0 and 1.

Nano storage uses various methods to fundamentally improve storage capacity and replace existing storage media with ultra-high-density media and devices. This is a major development direction for future storage devices.

DNA Data Storage - The Ultimate Density

Beyond nano-storage, **DNA data storage** is a prominent and promising area of research. It involves encoding digital binary data (0s and 1s) into the four chemical bases of synthetic DNA—Adenine (A), Cytosine (C), Guanine (G), and Thymine (T). This method offers unprecedented storage density, potentially capable of storing all of the world's data in a few kilograms of DNA. Furthermore, DNA is highly durable, offering a theoretical archival lifespan of hundreds of thousands of years, far surpassing current magnetic or optical media.

Cloud storage-storage technology that continues to evolve

Finally, I will briefly talk about cloud storage. Generally speaking, cloud storage is to store storage resources in a collection composed of many storage devices and servers. Users can connect to the "cloud" through any networkable device to conveniently access data anytime and anywhere.

Cloud storage.jpg

Cloud storage

Cloud storage supports the following two implementation modes:

Public cloud: Storage is provided by a third party as a service, and data is stored in a remote place. Users cannot control and do not understand the technology used in the cloud. It is common to use various cloud disks in our lives.

Private cloud: The data center develops internally for enterprises and provides cloud services, such as storage space application and rapid deployment of enterprise application systems.

Cloud storage improves storage efficiency and space utilization, and users can perform remote data backup and transmission at any time, reducing the cost of disaster recovery and backup units. At the same time, there are challenges such as data sovereignty and compliance, security risks (infringement, disclosure of personal privacy and commercial data), and the ongoing Total Cost of Ownership (TCO) model. In the context of the Internet of Everything and the sweeping wave of big data, cloud storage technology will continue to improve.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What are types of storage devices?

External storage devices

External HDDs and SSDs.

Flash memory devices.

Optical Storage Devices.

Floppy Disks.

Primary Storage: Random Access Memory (RAM)

Secondary Storage: Hard Disk Drives (HDD) & Solid-State Drives (SSD)

Hard Disk Drives (HDD)

Solid-State Drives (SSD)

2.What is a storage device give example?

Computer Storage Device Definition: A hardware device that can be used to store digital data and applications which may be in the form of images, video, audio, etc. is called a storage device. It is a key component of a computer and the hard drive is one of its examples.

3.What are five common storage devices?

Five common storage devices are:

USB flash drives.

Hard disks.

Optical disk.

RAM (volatile memory)

Floppy disk.
Related Articles

  • How to Use an External Hard Drive?
    How to Use an External Hard Drive?
    UTMEL24 June 20218975

    The external hard drive is a compact and portable hard drive storage which can be plugged in or unplugged at any time. It mainly uses USB or IEEE1394 interfaces. It can transmit data with the system at a higher speed. The IEEE 1394 interface transfer rate is 50-100 MB/s.

    Read More
  • Introduction to RAID (Redundant Arrays of Independent Disks)
    Introduction to RAID (Redundant Arrays of Independent Disks)
    UTMEL01 July 20218554

    RAID (Redundant Arrays of Independent Disks) means "a redundant array composed of independent disks". The RAID is the combination of many independent disks that combined into a large-capacity disk group. It uses the bonus effect of individual disks to provide data to enhance the performance of the entire disk system.

    Read More
  • What is NAND Flash?
    What is NAND Flash?
    UTMEL04 November 202111331

    NAND Flash is a better storage device than hard disk drives and is particularly evident in low-volume applications up to 4GB. As the quest continues for lower power consumption, lighter weight, and better performance, NAND is proving to be very attractive. Its development goal is to reduce the cost per bit of storage and increase storage capacity.

    Read More
  • Memory Chip: The Key to Smart Connectivity
    Memory Chip: The Key to Smart Connectivity
    UTMEL03 November 20212552

    In today's post, we talk about memory chips, especially their emerging applications in the AIoT smart interconnect space.

    Read More
  • Emerging Storage Technologies: MRAM, RRAM, and PCRAM
    Emerging Storage Technologies: MRAM, RRAM, and PCRAM
    UTMEL08 January 202611289

    The semiconductor industry is turning to emerging memories that offer higher storage performance, lower cost, and the ability to move toward process miniaturization. Three of these memories stand out -- MRAM, RRAM, and PCRAM.

    Read More