MEMS Basics: System Features and Classifications

Published: 11 June 2021 | Last Updated: 11 June 20216889
MEMS, also called micro-electro-mechanical system or micro-system, refers to high-tech devices with dimensions of a few millimeters or even smaller. The internal structure of MEMS is generally on the order of micrometers or even nanometers. A micro-electromechanical system is a micro-device or system that integrates micro-sensor, micro-actuator, micro-mechanical structure, micro-power supply, micro-energy, signal processing and control circuit, high-performance electronic integrated device, interface, and communication.
Watch to learn more about these tiny micro-electromechanical systems.

What is a MEMS (Micro-Electromechanical System)?

Catalog

Ⅰ Introduction
Ⅱ MEMS system Features
Ⅲ MEMS classifications1.Sensing MEMS technology
2.Biological MEMS technology
3.Optics MEMS technology
4.Radio frequency


Ⅰ Introduction

The MEMS is Micro Electromechanical System. It is mainly composed of three parts: sensors, actuators, and micro-energy. Micro electromechanical systems involve physics, semiconductors, optics, electronic engineering, chemistry, materials engineering, mechanical engineering, medicine, information engineering and biological engineering, and other disciplines and engineering technologies. It has opened up a wide range of applications such as intelligent systems, consumer electronics, wearable devices, and smart homes. Common products include MEMS accelerometers, MEMS microphones, micro motors, micro pumps, micro vibrators, MEMS pressure sensors, MEMS gyroscopes, MEMS humidity sensors, etc., and their integrated products. 

MEMS circuit.jpg

MEMS circuit

MEMS will have broad application prospects in the national economy and military systems. The main civilian fields are electronics, medicine, industry, automotive, and aerospace systems. In summary, MEMS has the following basic characteristics: miniaturization, intelligence, multi-function, high integration, and suitable for mass production.

Ⅱ MEMS system Features

MEMS (Micro-Electro-Mechanical System) was first used in automotive airbags, and then widely used in various fields of automobiles in the form of MEMS sensors. With the further development of MEMS technology. The demand for small-volume, high-performance MEMS products is increasing rapidly. MEMS products have also appeared in large numbers in consumer electronics, medical and other fields.

MEMS 2.png

MEMS

1) Miniaturization: MEMS devices are small in size, light in weight, low in energy consumption, low inertia, high in resonance frequency, and short in response time.

2) With silicon as the main material, the mechanical and electrical properties are excellent: the strength, hardness, and Young's modulus of silicon are equivalent to iron. The density is similar to aluminum, and the thermal conductivity is close to molybdenum and tungsten.

3) Mass production: With silicon micromachining technology, hundreds of micro-electromechanical devices or complete MEMS can be manufactured on a single silicon wafer at the same time. Mass production can greatly reduce production costs.

4) Integration: It can integrate multiple sensors or actuators with different functions, different sensitive directions or actuation directions, or form a microsensor array, a microactuator array, or even integrate devices with multiple functions. Form a complex microsystem. The integration of micro-sensors, micro-actuators, and microelectronic devices can produce highly reliable and stable MEMS.

5) Multidisciplinary: MEMS involves multiple disciplines such as electronics, machinery, materials, manufacturing, information and automatic control, physics, chemistry, and biology, and integrates many cutting-edge achievements in the development of science and technology today.

Ⅲ MEMS classifications

1.Sensing MEMS technology

Sensing MEMS technology refers to devices and systems that are processed by microelectronics and micromachines, and use sensitive components such as capacitors, piezoelectrics, piezoresistance, thermocouples, resonance, and tunnel current to sense and convert electrical signals. It includes various sensors such as speed, pressure, humidity, acceleration, gas, magnetism, light, sound, biology, chemistry, etc. According to the types, there are mainly: area array touch sensor, resonance force sensitive sensor, miniature acceleration sensor, vacuum microelectronic sensor, etc... 

MEMS sensor.jpg

MEMS sensor

The development of sensors is array, integration, and intelligence. Since the sensor is the tentacle for humans to explore the natural world and the neuron of various automated devices, it will be valued by countries all over the world in the future.

2.Biological MEMS technology

Biological MEMS technology is a chemical/biological micro-analysis and detection chip or instrument manufactured with MEMS technology. There is a micro-drive pump, micro-control valve, channel network, sample processor, mixing cell, metering, and augmentation manufactured on a substrate. Expanders, reactors, separators, detectors, and other components are integrated into a multifunctional chip. It can realize the whole analysis process of sample injection, dilution, reagent addition, mixing, amplification, reaction, separation, detection, and post-processing. It shrinks the traditional analytical laboratory functions on a chip. 

MEMES components.jpg

MEMES components

Biological MEMS system has the characteristics of miniaturization, integration, intelligence, and low cost. In terms of functions, it has the characteristics of a large amount of information, high analysis efficiency, few connections between the system and the outside, real-time communication, and continuous detection. Internationally, the research of biological MEMS has become a hot spot, and it will soon bring about a major innovation in biological and chemical analysis systems.

3.Optics MEMS technology

With the rapid development of information technology and optical communication technology, another field of MEMS development called micro-opto-electromechanical systems (MOEMS), that is, the integration of basic technologies such as microelectronics, micromechanics, and optoelectronics has appeared. It can completely integrate various MEMS structural parts with micro-optical devices, optical waveguide devices, semiconductor laser devices, photoelectric detection devices, etc. MOEMS has the characteristics of small size, low cost, mass production, precise driving, and control, etc. More successful applied scientific research mainly focuses on two aspects:

The first is a new display and projection equipment based on MOEMS, which mainly studies how to spatially modulate light through the physical movement of the reflecting surface. Typical representatives are digital micromirror array chips and grating light valves. The second is communication systems, which mainly research through micromirrors. The physical movement of the optical path is used to control the expected change of the optical path. The more successful optical communication devices such as optical switch modulators, optical filters, and multiplexers. MOEMS is a highly comprehensive and highly interdisciplinary high-tech. Carrying out scientific and technological research in this field can drive the development of a large number of new concept functional devices.

4.Radio frequency

Radio frequency MEMS technology is traditionally divided into two types, fixed and movable. Fixed MEMS devices include body micro-machined transmission lines, filters, and couplers, and movable MEMS devices include switches, tuners, and variable capacitors. According to the technical level, it is divided into: 1. The basic device-level composed of micromechanical switches, variable capacitors, and inductive resonators; 2. The component level composed of phase shifters, filters, and VCOs; 3. The application system-level composed of variable beam radar phased array radar antennas, etc. With the passage of time and the gradual development of technology, the content of MEMS is constantly increasing and becoming more abundant.

The world-famous information technology journal "IEEE Proceedings" summarized the content of MEMS in the 1998 MEMS album as integrated sensors, microactuators, and microsystems. People also classify micromachines, microstructures, and smart sensors into the category of MEMS. The technology of making MEMS includes two parts: microelectronics technology and micromachining technology. The main contents of microelectronics technology are: oxide layer growth, photolithography mask production, photolithography selective doping (shielding diffusion, ion implantation), thin-film (layer) growth, connection production, etc. The main content of micro-processing technology includes silicon surface micro-processing and silicon body micro-processing (anisotropic corrosion, sacrificial layer) technology, wafer bonding technology, and LIGA technology for making high-aspect-ratio structures. The use of microelectronics technology can manufacture integrated circuits and many sensors. Micromachining technology is very suitable for making certain pressure sensors, acceleration sensors, micro pumps, microvalves, micro grooves, micro reaction chambers, microactuators, micro machines, etc. This can give full play to the advantages of microelectronics technology and use MEMS Technology manufactures high-reliability micro-satellites in large quantities and at low cost.

MEMS technology is an emerging technology field, mainly belonging to the category of micron technology. The development of MEMS technology has gone through more than 10 years. Most of them are based on the existing technology and are manufactured with technological approaches from large to small. A number of new integrated devices have been developed, which greatly improved the function and efficiency of the devices. The development of MEMS technology may, like microelectronics, have a revolutionary impact on science and technology and human life, especially for the development of micro-satellites, which will open the door to mass production of low-cost, high-reliability micro-satellites.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What are the types of MEMS?

There are two types of MEMS accelerometers: variable capacitive and piezoresistive. Variable capacitives are highly sensitive and piezoresistive are low range devices used for acceleration measurement.

2.What is the importance of MEMS?

Micro/NanoElectroMechanical Systems (MEMS) technology offers the opportunity to produce mechanical, electromechanical, and electrochemical devices with the same unprecedented levels of miniaturization, and functionality as modern very large scale integrated (VLSI).

3.How does a MEMS sensor work?

MEMS is a chip-based technology, known as a Micro-Electro-Mechanical System. Sensors are composed of a suspended mass between a pair of capacitive plates. When the tilt is applied to the sensor, the suspended mass creates a difference in electric potential. The difference is measured as a change in capacitance.

4.What is MEMS and its applications?

MEMS are low-cost, and high accuracy inertial sensors, and these are used to serve an extensive range of industrial applications. This sensor uses a chip-based technology namely a micro-electro-mechanical system. Additionally, these sensors use a particular process like micromachining.

5.Who invented MEMS?

Harvey C. Nathanson

Nathanson (October 22, 1936 – November 22, 2019) was an American electrical engineer who invented the first MEMS (micro-electro-mechanical systems) device of the type now found in products ranging from iPhones to automobiles.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242456

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • A Comprehensive Guide to FPGA Development Boards
    A Comprehensive Guide to FPGA Development Boards
    UTMEL11 September 202514082

    This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20253485

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • 800G Optical Transceivers: The Guide for AI Data Centers
    800G Optical Transceivers: The Guide for AI Data Centers
    UTMEL24 December 20253522

    The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.

    Read More
  • Xilinx FPGAs: From Getting Started to Advanced Application Development
    Xilinx FPGAs: From Getting Started to Advanced Application Development
    UTMEL09 September 20254198

    This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.

    Read More