Introduction to IC Packaging

Published: 06 November 2021 | Last Updated: 08 January 202616707
In recent years, IC packaging technologies have emerged and new terms have emerged. There are at least a few dozen IC packaging-related names that can be listed.
This video introduces you to IC Packaging.

Introduction to IC Packaging

2026 Executive Summary: Advanced IC packaging has evolved from a secondary manufacturing step to a primary driver of Moore's Law. In 2026, the industry distinguishes between XY plane extension (utilizing RDL for thinner, mobile-first designs like FOWLP) and Z-axis extension (utilizing TSV for high-performance computing like CoWoS and HBM4). This guide details the 12 critical packaging technologies powering today's AI accelerators and 5G/6G devices.        

Catalog

IC packaging based on XY plane extension

 

FOWLP

INFO

FOPLP

EMIB

IC packaging based on Z-axis extension

 

CoWoS

HBM

HMC

Wide-IO

Foveros

Co-EMIB (Foveros + EMIB)

SoIC

X-Cube

Summary


In 2026, the semiconductor industry classifies IC packaging into two primary architectures based on signal interconnection direction:

  • XY Plane Extension: Packaging technologies that extend signals horizontally using Redistribution Layers (RDL) without penetrating the silicon substrate.

  • Z-Axis Extension: 2.5D and 3D packaging technologies that utilize Through-Silicon Vias (TSV) to stack chips vertically for high-bandwidth communication.

1. What is XY Plane Extension Packaging?

XY plane extension refers to packaging techniques that expand signal connectivity across the horizontal plane of the wafer or chip without vertical stacking.

Key Characteristics: The distinctive feature of this category is the absence of TSV (Through-Silicon Vias). Instead, signal extension is achieved through RDL (Redistribution Layers) attached directly to the silicon body or molding compound. By eliminating the organic substrate, these packages achieve the ultra-thin profiles required for modern smartphones and wearable technology.

FOWLP (Fan-Out Wafer Level Package)

Definition: FOWLP is a variation of Wafer Level Packaging (WLP) where the package area is larger than the chip itself, allowing for more I/O connections.

To understand FOWLP, we must look at the evolution of WLP technology. Introduced around 2000, WLP represented a shift where packaging occurred before wafer dicing. WLP is categorized into two types:

  • Fan-In WLP: The package size is equal to the chip size (Chip Scale Package or CSP). Ideal for low-pin-count devices.

  • Fan-Out WLP (FOWLP): As IC processes shrunk to 3nm and beyond, chip areas became too small to accommodate the necessary number of solder balls. FOWLP utilizes RDL to "fan out" connections beyond the chip's edge, enabling high I/O counts in a minimal footprint.

The standard FOWLP workflow involves reconstructing diced good dies on a carrier wafer before applying the RDL and molding compound, as shown below.

FOWLP Packaging Process Diagram showing reconstitution and RDL formation

Figure 1: FOWLP Packaging Process

InFO (Integrated Fan-out)

InFO is TSMC's proprietary evolution of FOWLP technology, designed to integrate multiple chips within a single fan-out package without a substrate.

While standard FOWLP focuses on single-die packaging, InFO facilitates high-density integration for RF components, processors, and baseband chips. It drastically reduces package thickness and improves thermal performance.

Schematic comparing FIWLP, FOWLP and TSMC InFO structures

Figure 2: Evolution from FIWLP to InFO

Industry Impact: TSMC's InFO technology was the decisive factor in securing exclusive orders for Apple's A-series processors starting with the A10 and continuing through the 2026 A-series chips. By eliminating the substrate, InFO allows for thinner iPhones and larger battery capacities, setting the standard for premium mobile packaging.

FOPLP (Fan-out Panel Level Package)

FOPLP transfers the FOWLP process from circular silicon wafers to large-area rectangular panels to achieve economies of scale.

As of 2026, FOPLP typically utilizes 610×457mm PCB carrier panels. This area is approximately four times larger than a standard 300mm (12-inch) silicon wafer, allowing for 4x higher throughput per batch.

Visual comparison of 300mm Wafer area versus FOPLP Panel area

Figure 3: Area comparison of FOWLP vs. FOPLP

While FOPLP offers significant cost reductions (using PCB-based RDL with >10um line widths), it faces challenges with panel warpage. However, major players like Samsung Electronics and ASE are aggressively expanding FOPLP capacity for power management ICs and mid-range processors to reduce costs.

EMIB (Embedded Multi-Die Interconnect Bridge)

EMIB is Intel's heterogeneous integration technology that bridges two or more silicon dies embedded within a standard substrate.

Unlike 2.5D packages that require a large, expensive silicon interposer, EMIB uses a tiny silicon bridge only where high-density interconnection is needed. This makes it a cost-effective "substrate-class" package that acts as a middle ground between standard organic packages and full 2.5D integration.

Key Advantage: EMIB allows the "Mix and Match" of different process nodes. A 2026 Intel processor might combine a 1.8nm (18A) CPU tile, a 3nm GPU tile, and a legacy node I/O tile into a single package.

Cross-section of Intel EMIB showing the embedded silicon bridge in the substrate

Figure 4: EMIB Structure

2. How does Z-Axis (3D) Packaging Work?

Z-axis extension technologies utilize TSV (Through-Silicon Via) to create vertical signal pathways through the silicon die itself. This enables 2.5D and 3D stacking, essential for high-performance computing (HPC) and AI applications.

By shortening the interconnect length between chips, TSVs reduce latency and parasitic capacitance, allowing for higher frequencies and lower power consumption compared to wire bonding or long planar traces.

CoWoS (Chip-on-Wafer-on-Substrate)

CoWoS is TSMC's premier 2.5D packaging technology. It involves mounting logic chips and High Bandwidth Memory (HBM) side-by-side on a silicon interposer, which is then bonded to a package substrate.

Diagram of CoWoS showing logic and memory on a silicon interposer

Figure 5: CoWoS Architecture

2026 Status: CoWoS is the backbone of the AI revolution. It is the packaging technology used for NVIDIA's Blackwell and Rubin AI accelerators, as well as high-end chips from AMD and Google TPU. The interposer allows for thousands of high-density connections between the GPU and HBM, delivering the massive memory bandwidth required for Large Language Models (LLMs).

HBM (High-Bandwidth Memory)

HBM stacks DRAM dies vertically using 3D TSVs to achieve exceptional bandwidth. These stacks are then connected to a processor (GPU/CPU) via a 2.5D interposer.

3D view of HBM memory stack connected to a GPU via interposer

Figure 6: HBM Structure

Evolution to 2026: While early versions like HBM2 offered ~256 GB/s, the current standard HBM3E and the emerging HBM4 deliver bandwidths exceeding 1.2 TB/s per stack. Leading manufacturers SK Hynix, Samsung, and Micron drive this technology, providing the memory subsystems critical for generative AI performance.

HMC (Hybrid Memory Cube) - Legacy Tech

HMC was a 3D memory standard promoted by Micron that integrated the memory controller directly into the DRAM stack using TSVs.

HMC structure showing stacked DRAM and logic base

Figure 7: HMC (Legacy)

While HMC pioneered TSV usage in memory, the industry largely coalesced around the HBM standard (JEDEC) for high-performance graphics and AI, leading to HMC's discontinuation. However, HMC's architecture influenced modern 3D stacking techniques.

Wide-IO

Wide-IO is a mobile-focused 3D stacking technology where memory chips are mounted directly on top of the logic (processor) chip using TSVs.

Wide-IO structure showing memory stacked on logic

Figure 8: Wide-IO

This vertical integration minimizes the path length for data, significantly reducing power consumption—a critical factor for smartphones and tablets.

Foveros (3D Face-to-Face Stacking)

Foveros is Intel's active 3D stacking technology. Unlike 2.5D packaging (EMIB), Foveros stacks logic die upon logic die.

In architectures like Meteor Lake and Arrow Lake, Foveros allows a high-performance compute tile to be stacked on a low-power base die containing I/O and cache. This maximizes space efficiency and allows different IP blocks to be manufactured on their optimal process nodes.

Foveros packaging diagram showing active die on active die

Figure 9: Foveros 3D Stacking

Co-EMIB (Foveros + EMIB)

Co-EMIB combines the vertical stacking of Foveros with the horizontal interconnection of EMIB.

This creates highly complex systems, such as the Ponte Vecchio GPU, where multiple 3D stacks (Foveros) are connected horizontally via bridges (EMIB). It utilizes ODI (Omni-Directional Interconnect) to provide robust power delivery and communication between layers.

Diagram showing combination of Foveros and EMIB

Figure 10: Co-EMIB Architecture

SoIC (System-on-Integrated-Chips)

SoIC is TSMC's front-end 3D packaging technology that uses Hybrid Bonding (bumpless bonding).

Unlike CoWoS (which connects finished chips), SoIC bonds wafers or chips directly copper-to-copper without solder bumps. This allows for extremely dense vertical connections (sub-micron pitch) and practically zero signal loss. It is currently deployed in AMD's MI300 series data center accelerators.

Comparison of bump pitch in 3D IC versus bumpless SoIC

Figure 11: SoIC vs. Traditional 3D IC

X-Cube

X-Cube is Samsung's 3D integration solution utilizing TSV technology to stack SRAM or memory directly on top of logic.

Targeting 5G, AI, and HPC markets, X-Cube enables significant reductions in die footprint while maximizing speed. It supports Samsung's advanced 5nm and 3nm GAA (Gate-All-Around) process nodes.

Exploded view of Samsung X-Cube

Figure 12: X-Cube

3. Summary: The Future of Chip Packaging

The past 15 years have transformed packaging from a protective shell into a performance multiplier. The table below compares these mainstream technologies.

Table comparing various packaging technologies by type and application

Conclusion: As we move through 2026, the demand for AI computation and energy efficiency ensures that advanced packaging (CoWoS, SoIC, Foveros) will remain as critical as the lithography node itself. The goal remains constant: Improve functional density, shorten interconnects, and reduce power consumption.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is IC packaging and testing?

In electronics manufacturing, integrated circuit packaging is the final stage of semiconductor device fabrication, in which the block of semiconductor material is encapsulated in a supporting case that prevents physical damage and corrosion. The packaging stage is followed by testing of the integrated circuit.

2.Why is IC packaging important?

IC packaging is the ability to provide more and more I/O interconnections to a die (bare chip) that is increasingly shrinking in size is an ever-present problem. This will imposes challenges for new 3D integration that requires innovative packaging technologies.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242456

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • A Comprehensive Guide to FPGA Development Boards
    A Comprehensive Guide to FPGA Development Boards
    UTMEL11 September 202514082

    This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20253485

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • 800G Optical Transceivers: The Guide for AI Data Centers
    800G Optical Transceivers: The Guide for AI Data Centers
    UTMEL24 December 20253522

    The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.

    Read More
  • Xilinx FPGAs: From Getting Started to Advanced Application Development
    Xilinx FPGAs: From Getting Started to Advanced Application Development
    UTMEL09 September 20254198

    This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.

    Read More