The Comprehensive Guide to MOSFETs: Principles, Types, and Parameters (2026 Edition)

Published: 12 March 2022 | Last Updated: 16 January 202617965
Hello everyone, I am Rose. Today I will introduce MOSFET to you. Metal-Oxide Semiconductor Field Effect Transistor (MOSFET) is a field effect transistor that can be widely used in analog circuits and digital circuits
This video completely explains the structure, channel formation, current flow, characteristics, pinch-off effect, and circuit symbols of MOSFET.

How Does a MOSFET Work?

Key Takeaways

  • Definition: MOSFET (Metal-Oxide-Semiconductor Field-Effect Transistor) is a voltage-controlled device used for switching and amplification.

  • Key Advantage: High input impedance, low power consumption, and fast switching speeds compared to BJTs.

  • Types: Divided into N-Channel/P-Channel and Enhancement/Depletion modes.

  • Selection: Use MOSFETs for high-frequency, low-voltage (<600V) applications; use IGBTs for high-voltage/current.

The MOSFET is a fundamental semiconductor device that utilizes the field effect principle to control current. Compared to traditional bipolar transistors (BJTs), MOSFETs offer high input impedance, low noise, wide dynamic range, and ease of integration.

They are ubiquitous in modern electronics, powering everything from computer power supplies (Switching Power Supplies) to high-frequency inverters and communication devices.

Types and Structure of MOSFETs

MOSFETs act as a specific type of FET (Field Effect Transistor). They are categorized into four distinct types based on their channel and mode of operation:

  • N-Channel Enhancement Mode (Most common)

  • N-Channel Depletion Mode

  • P-Channel Enhancement Mode

  • P-Channel Depletion Mode

4 Types of MOS Tubes Classification Chart

Figure 1: The 4 Classifications of MOSFETs

Every MOSFET has three main electrodes:

  1. G (Gate): The control pin.

  2. S (Source): The current source.

  3. D (Drain): The current output.

Internal Structure of MOS Tube

Figure 2: Internal Structure of a MOSFET


Ⅰ. MOSFET Working Principle

1. N-Channel Enhancement Mode

This is the most widely used structure. It involves two highly doped N-type regions diffused onto a P-type substrate.

  • When VGS = 0: No current flows because the P-substrate creates back-to-back PN junctions between the Drain and Source.

  • When VGS > 0: A positive voltage at the Gate attracts electrons to the surface of the P-substrate. When this voltage exceeds the Threshold Voltage (Vth), an "inversion layer" forms, creating a conductive N-channel connecting the Drain and Source.

Schematic of N-channel Enhancement Mode MOS Transistor

Figure 3: N-Channel Enhancement Mode Structure (OFF vs ON)

Pinch-off Effect: As the Drain-to-Source voltage (VDS) increases, the channel becomes tapered. If VDS becomes too high, the channel "pinches off" near the drain, limiting the current. This is the saturation region.

Depletion Layer and Inversion Layer Structure

Figure 4: Formation of the Conductive Channel

Pre-pinch-off and Pinch-off Area formation

Figure 5: The Pinch-off Phenomenon

2. P-Channel Enhancement Mode

The operation is the inverse of the N-Channel. It is built on an N-type substrate. To turn it on, the Gate voltage must be lower than the Source voltage (negative VGS) to attract holes and form a channel.

P-channel Enhancement Mode Structure

Figure 6: P-Channel Enhancement Mode Structure

P-channel Depletion Layer Formation

Figure 7: P-Channel Channel Formation

P-channel Pinch-off

Figure 8: P-Channel Pinch-off Region

3. Depletion Mode (N & P)

Unlike enhancement mode, Depletion Mode MOSFETs are "Normally ON" devices. A channel is physically implanted during manufacturing. They conduct current when VGS = 0. To turn an N-Channel depletion MOS off, you must apply a negative gate voltage.

Note: Enhancement mode MOSFETs are preferred in 99% of modern power applications (like switching power supplies) because "Normally OFF" is safer for circuit design.

N-channel Depletion-mode MOS Transistor Structure

Figure 9: Depletion Mode Structure and Transfer Characteristics


Ⅱ. Important Characteristics of MOSFETs

1. Switching (Conduction) Characteristics

  • NMOS: Turns ON when VGS > Vth. Used for Low-Side Switching (Source connected to GND).

  • PMOS: Turns ON when VGS < Vth. Used for High-Side Switching (Source connected to VCC).

2. Loss Characteristics

MOSFET efficiency is defined by two types of losses:

  • Conduction Loss: Caused by the internal resistance ($R_{DS(on)}$) when the device is on. $P = I^2 \times R_{DS(on)}$.

  • Switching Loss: Occurs during the transition between ON and OFF states. Higher frequency = Higher switching loss.

3. Parasitic Capacitance & Driving

MOSFETs have parasitic capacitances (Cgs, Cgd, Cds). Driving a MOSFET essentially means charging and discharging these capacitors. The Miller Effect (Cgd) significantly impacts switching speed.

Comparison of Characteristics of 4 Kinds of MOS Tubes

Figure 10: Comparison of MOSFET Types

4. Parasitic (Body) Diode

All discrete power MOSFETs have an intrinsic body diode between the Drain and Source. This is crucial for inductive load driving (like motors) as it provides a freewheeling path for current protection.

Parasitic Body Diode Position

Figure 11: Position of the Parasitic Body Diode


Ⅲ. MOSFET vs. BJT vs. IGBT

Understanding when to use which device is critical for circuit design.

1. MOSFET vs. BJT (Triode)

FeatureBJT (Bipolar Junction Transistor)MOSFET
Control TypeCurrent Controlled (Requires Base Current)Voltage Controlled (Requires Gate Voltage)
Switching SpeedSlower (Storage time issues)Very Fast (No carrier storage time)
Input ImpedanceLowVery High
Carrier TypeBipolar (Electrons & Holes)Unipolar (Majority carriers only)
Thermal StabilityRisk of Thermal Runaway (Negative Coeff)Good (Positive Temp Coeff - Self regulating)

2. MOSFET vs. IGBT

The IGBT (Insulated Gate Bipolar Transistor) is a hybrid device combining the input characteristics of a MOSFET (Voltage drive) with the output characteristics of a BJT (High current capability).

  • Low Voltage (< 600V) & High Frequency: MOSFETs are superior due to lower switching losses and linear conduction voltage drop.

  • High Voltage (> 600V) & High Current: IGBTs are superior. They handle high voltages better but switch slower than MOSFETs.


Ⅳ. Main Parameters of MOSFETs

When reading a datasheet, focus on these critical specifications:

1. Absolute Maximum Ratings

  • $V_{DSS}$ (Drain-Source Breakdown Voltage): The maximum voltage the device can withstand before breakdown.

  • $V_{GS}$ (Gate-Source Voltage): Maximum voltage for the Gate oxide layer (usually ±20V). Exceeding this destroys the device.

  • $I_D$ (Continuous Drain Current): Maximum current the chip can handle at a specific case temperature.

  • EAS (Single Pulse Avalanche Energy): The device's ability to absorb transient energy (voltage spikes).

Maximum Drain Current Graph

Figure 16: Drain Current Limits

Avalanche Damage Endurance Test Circuit

Figure 17: Avalanche Test Circuit

2. Static Characteristics

  • $R_{DS(on)}$ (On-Resistance): The most critical efficiency parameter. Lower resistance means less heat and less power loss.

  • $V_{GS(th)}$ (Threshold Voltage): The voltage required to start conducting. Logic level MOS (3.3V/5V) has lower thresholds.

3. Dynamic Characteristics

  • $Q_g$ (Total Gate Charge): The amount of charge required to turn the MOSFET on. Lower $Q_g$ enables faster switching speeds.

  • $C_{iss}$ (Input Capacitance): Affects how much current the driver needs to supply.

  • SOA (Safe Operating Area): A graph defining the safe combinations of Voltage and Current to avoid device destruction.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. What does mosfet mean?

Metal-Oxide Semiconductor Field Effect Transistor, (MOSFET). It is a field-effect transistor that can be widely used in analog circuits and digital circuits.

2. Where are MOSFETs used?

1. Field effect tube can be used for amplification. Since the input impedance of the FET amplifier is high, the coupling capacitor can be small, and the electrolytic capacitor is not necessary.
2. The high input impedance of the FET is very suitable for impedance transformation. It is often used in the input stage of multi-stage amplifier for impedance transformation.
3. The FET can be used as a variable resistor.
4. The FET can be easily used as a constant current source.
5. FETs can be used as electronic switches.

3. What is the difference between MOSFET-P and MOSFET-N?

1. MOSFET-P is P-channel, MOSFET-N is N-channel;
2. In order to work normally, the external Vds of the NMOS tube must be a positive value, the turn-on voltage VT must also be a positive value, and the actual current direction is flowing into the drain.
Unlike NMOS, the external Vds of the PMOS tube must be a negative value, the turn-on voltage VT must also be a negative value, and the actual current direction is to flow out of the drain.
N-channel and P-channel MOSFETs are classified into enhancement mode and depletion mode.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242456

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • A Comprehensive Guide to FPGA Development Boards
    A Comprehensive Guide to FPGA Development Boards
    UTMEL11 September 202514087

    This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20253488

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • 800G Optical Transceivers: The Guide for AI Data Centers
    800G Optical Transceivers: The Guide for AI Data Centers
    UTMEL24 December 20253525

    The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.

    Read More
  • Xilinx FPGAs: From Getting Started to Advanced Application Development
    Xilinx FPGAs: From Getting Started to Advanced Application Development
    UTMEL09 September 20254199

    This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.

    Read More